Other Parts Discussed in Thread: TVP5158, DM385
We are developing custom application using IPNC RDK 3.5 version. we have developed one custom chain to capture video from AR330 sensor along with 3 CVBS input video from TVP5158. If we capture video(Full HD) from AR0330 sensor alone, the video capture, display, encode and streaming are working fine without any issue. But after integrating with 3 CVBS video, the full HD video is not smooth but analog video are fine. Only Full HD video is flickering and it seems the old frames are displayed in between the latest frames.
As we are not using TILER_MEMORY, We have changed the memory map to reduce the TIMER memory to 16MB and increased the SR2 region to 217MB.
Attached the log file for more information.