Current understanding is that he PMIC first turns on and performs the Power on sequence with the voltage values configured according to the OTP used. Once the J6 boots up, it changes the various PMIC voltages according to its own programmed AVS settings.
Question - Is this configuration of the PMIC, already implemented as part of the GLSDK ? Or should a customer explicitly implement this in the application that they develop on the GLSDK ?