This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am3359 using ecap to capture synchronized input

Other Parts Discussed in Thread: AM3359

Hi, 

I am trying to figure out if I can use the ECAP on the AM3359 to capture serial input synchronously on the rising edge of a clock (1.3kHz clock). This is a custom protocol.

It is a serial protocol that send data to the AM3359, the data is sent from the external device on the rising edge of a clock. I want to sample the data line from the external device using the ecap every time a rising edge occurs on the clock.

I have been reading through the ECAP and from what I understand it has a synchronous input mode. 

Do you think this is possible using the ECAP?

Regards