This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Embedded board selection

Hi,

I am presently on drawing board for a product development and need to work on selecting an embedded board with the following specs.

1. CPU 500MHz or above

2. 02 nos. Ethernet Ports

3. Flash 2 MB or above

4. RAM 1 MB OR above

I will be Ok with the option of using a CPU board (with CPU & Memory space only) and a breakout board with the Dual Ethernet Ports.

Or all on-board. However, want to select a board with the above minimum specs. 

Will appreciate if  I get support from the forum to accomplish my selection.

Thanks in anticipation !!