Hello all,
I am using CCS 5.5 and C6678 DSP.
All cores 1-7 will run the same code (similar to the image demo project) with the exception that each core will have a different section of the DDR3.
Question: How can we use the same .cfg file and inside the file, based on the core number (DNUM), select a different DDR3 section
Something like this
if (DNUM==1)
{
Program.sectMap[".text"] = "DDR3CORE1";
else if (DNUM==2)
Program.sectMap[".text"] = "DDR3CORE2";
...
}
This is needed so we can use the same .out file with the MAD which will reduce the firmware size alot
Regards,
Murad