Other Parts Discussed in Thread: AM3352
Hi!
We designed custom single-board controller around am3352 SoC. We uses NAND chip by Micron as general storage.
At first generation of design there was a MT29F4G08ABADA (4Gb ~ 512MB), and everything was fine.
We used u-boot build "freezed" at tag 2013.07 with some changes concerns our board, and
left it "as is" for a years.
But now we need modification with more disk space, and we decided to use MT29F16G08ABABA chip (16Gb ~ 2GB).
Suddenly ( :-) ) new board began to fail with this chip! Some investigations... and I (I am programmer in our workgroup) see,
that old u-boot failed at NAND detection. And there was huge code for the 3 years, including ONFI NAND support. And also
linux like Kbuild configuration, driver model an so on.
Something else... We use 2 builds of u-boot:
1. "Fabrication" (in other words "debrick") build, that boots over dhcp/tftp, and automaticly writes NAND partitions from MLO to kernel.
2. "Main"-standalone build, that boots from NAND.
Ok, I got fresh u-boot clone from denx.de , dragged our custom code to new source-tree, and now we have:
- "Fabrication" build - seems works fine, and I can see how it processes at console, there are no errors, except messages like this:
CACHE: Misaligned operation at range [81000000, 81059672]
- NAND chip detection - OK;
- u-boot "nand info" command, it seems, shows correct:
=> nand info
Device 0: nand0, sector size 512 KiB
Page size 4096 b
OOB size 224 b
Erase size 524288 b
subpagesize 1024 b
options 0x4000000c
bbt options 0x 0
- "nand write" operation reports "OK";
- nand read partition ok, and md shows correct hexdump (at few start segments that we can check by eyes)
But after debrick.scr script execution, which ends with "go 20000;" (ROM code address, isnt?)
We have:
## Starting application at 0x00020000 ...
prefetch abort
pc : [<00020004>] lr : [<8ff700b5>]
reloc pc : [<f08b1004>] lr : [<808010b5>]
sp : 8ef44cf8 ip : 8ef44ad4 fp : 8ffb69e0
r10: 00000002 r9 : 8ef4eed8 r8 : 00000000
r7 : 8ef96330 r6 : 00020000 r5 : 00000002 r4 : 8ef96334
r3 : 00020000 r2 : 8ef96334 r1 : 8ef96334 r0 : 00000001
Flags: nzCv IRQs off FIQs on Mode SVC_32
Resetting CPU ...
Any suggestions?
Thanks for help, ideas... right questions.