During a schematic Design Review, the following comment was made: Refer to AM335x Errata – Advisory 1.0.30. OSC_GND and RTC_GND should not be isolated grounds and you should connect the VSS_OSC and VSS_RTC terminals and respective crystal circuit component grounds directly to the common PCB digital ground plain. .
If the GNDs are not connected together, and the OSC components are not tied directly to the GND plane, could this cause RTC RESET when switched to RTC-only mode? What we are seeing with this design is an occasional RTC being cleared (RESET) when changing either TO or FROM RTC-only mode.
~Leonard
.