why I set '#define TWO_EMIF 0' in DM8168.gel file, when I use ddr test code write data to the EMIF1, there are still data in EMIF1?
for example:
#define TWO_EMIF 0 /*0: EMIF0 only Enabled 1: Both the EMIFs are enabled */
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi xiu,
When you write data to EMIF1, there will be data to EMIF1.
Regards,
Pavel