This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

For Active-Noise-Reduction which Developer-Kit?

Other Parts Discussed in Thread: TMDSLCDK6748, OMAP-L138, TMDSLCDK138, OMAPL138

Hi Everyone,

For my Master-project I want to test in which area an Active-Noise-Reduction is useful.

But for this i need a Kit, which can solve the FxLMS-Algorithm and the FIR-Filter. I get an old TMS320C6711 DSB-Board from my University.

But I need a newer one, so i can Programm it whith windows 7. I don't have such an old PC. So I want to know, if there is an Developer Kit, which can solve my Problem, has 2 Microphone Inputs, one Speaker Output and it is possible to programm it with Ethernet or USB-Cable.


Best Regards,

Jan

  • Hi, Jan,

    Welcome to E2E and thank you for your interest in our products!

    I'm moving your post to the C67x Single Core DSP Forum. They have more experience on this device.

    Best regards,
    Luis Fernando Rodríguez S.
  • Jan,

    Please take a look at the TMDSLCDK6748 or the TMDSLCDK138. The OMAP-L138 is the same as the C6748 but has an added ARM9 core that can run Linux. You can use the LCDK138 in place of the LCDK6748 and just ignore the ARM9 if you want to have the flexibility to use the ARM9 later.

    You will need to purchase a low-cost JTAG emulation pod such as the TMDSEMU100v2U-14T. Be sure to get one with the 14-pin TI header. Others come with some other connectors instead, but you will need the TI 14-pin header for either LCDK.

    Regards,
    RandyP
  • Hi Jan,

    In addition to Randy's suggestions,

    The C6748 LCDK/OMAPL138 LCDK kit comes along with good software packages and "TI C6000 DSPLIB". The DSPLIB is an optimized DSP Function Library for C programmers. It includes many C-callable, optimized, general-purpose signal-processing routines. These routines are typically used in computationally-intensive real-time applications where optimal execution speed is critical.

    It has sample examples to demonstrate the FIR as well.