This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Adding a header to my program stops working



Hello everyone,

first of all... my system:

Win7, CS5v5, TMS320C6713, DSK6713

If am adding the white_noise.h, my program doenst work anymore! I dont use it.. just adding to my program. 
If Im comment this line with my header... my program stil works.

Who has a idea ?^^

Its very strange... 

thank you so much!

greetings

daniel 

MAIN.C

#include "header.h"
#include "DSK6713_AIC23.h"
//#include "white_noise.h"      <<<<<<<<<<<< If this still uncomment works my program, if not -> nothing happens


Uint32 fs= DSK6713_AIC23_FREQ_8KHZ;

//Define
#define LEFT 0						//stereo
#define RIGHT 1						//stereo

int i=0;
//Data Transfer from/to Codec
union {Uint32 combo; short channel[2];} AIC23_data;
union {Uint32 uint; short channel[2];} AIC23_input;
short x[3] = {0,0,0};
short input;

interrupt void c_int11()	    //ISR
{
	DSK6713_LED_on(0);

//function call for NLMS Function
	output=NLMS_function();
	 output_sample(output);	            //overall output result



	x[1] = x[0];
	x[0] =IR[i];
	output_sample(x[0]);
	if(i < 7999) ++i;
	else
		i=0;


	AIC23_input.uint = input_sample();
		input = (short)(AIC23_input.channel[RIGHT] + AIC23_input.channel[LEFT]);



*/



	 DSK6713_LED_off(0);
	 return;					//return from ISR
}

main()
{
	DSK6713_LED_init();  						//init LEDs

	 short T=0;
	 for (T = 0; T < 30; T++)
	   {
	     w[T] = 0;			      //init buffer for weights
	     delay[T] = 0;		      //init buffer for delay samples
	   }
	 comm_intr();                       //init DSK, codec, McBSP
	 while(1);                          //infinite loop             			    		//infinite loop
}

white_noise.h

 short IR[8000]={23670, -2424, -25025, 23474, 32467, -10922, -5724, -11739, 22429, 26085, 23263, -15212, -14811, 28867, 25562, 2802, 7969, -25847, -7053, 14004, -21983, -6196, -11253, -29670, 18716, 21662, -4035, -23656, 30805, 29325, 10274, 30720, 6561, 10053, -21803, 731, -14502, -14133, -26843, -13453, -8523, 9494, -31533, -16858, -9279, 3350, -15128, 18635, 30184, 14327, -20427, 21975, -28405, -5996, -7438, -23874, 4640, 12456, -32392, 27224, -11279, -16896, 16588, 15481, -28716, -20265, 219, 18118, -23586, 4008, -26563, 22332, 7765, 15156, 23383, 22896, 7371, -32718, 28359, 27032, -28826, 22905, 14708, 12375, -16851, 17438, -26772, -19181, 27089, -18746, 24602, -1192, 10646, 7382, 7914, 824, -18724, 8024, -11379, 5998, -15505, 13400, -15281, -6865, -30446, -15542, 18234, -232, -11, 14862, -25160, 14466, 4777, -2586, -24097, 18403, -28977, -10885, -18074, -16409, -27266, -13376, -4332, 2259, 20926, 545, -18657, -27071, 3619, -25476, 10615, 12198, -8793, -7884, -29054, 17936, 5017, 5600, -3903, -947, 16522, 20705, -10924, 28327, -28537, 8485, -4171, 20622, 23830, -14819, 9186, 21105, -32486, 13508, -14491, -18760, -22260, 10961, 19886, -20010, -27883, -4323, 27523, -21073, 946, -22853, -19988, -30038, 12239, -15117, -14270, -5100, -12630, -16637, -30253, -29235, -18004, 25127, -842, -3487, 4123, -17201, -32066, 781, 13141, -10522, -1461, -24130, -24645, 9074, -9925, 31638, -18717, 5071, -25603, 27171, -21453, -29429, -5384, -13357, -18318, -15222, 30532, -27565, -5040, -23953, -28102, 4412, -8606, -5322, 503, 1392, 17606, -9752, 18509, 9334, 8908, -15757, -25977, 16245, -22390, -17498, -23650, 7205, -31376, 25110, -32217, -11741, -22214, 28540, -6472, -6679, -32095, 24080, 15083, -6033, -18871, -21766, 23742, 12991, 7742, -10457, -24815, 398, -19865, -24120, -16139, 11064, -25662, -11507, 25328, 6538, -25787, -4638, -20215, 288, -21009, -12333, 8251, -21242, 17173, -27094, 748, -22049, -30481, -32090, 4940, 32589, 6954, -6061, 27208, 14455, 6112, -7691, -30491, -10707, 13141, 19877, -30352, -31969, -21217, 31421, 19459, -42, 8551, -7437, -14175, 21413, 5186, 7898, 18771, 1062, 29804, -24664, 21991, -25419, -15862, 18767, -20208, 20977, 29615, 3017, -27107, -7356, -11089, 17950, -28744, 2555, 12135, -4938, 21912, 24210, -7429, -24113, 316, -4380, 17685, -16104, 15337, 19655, -14517, 8441, 9212, -17475, 23400, -3897, -589, -31655, 966, -15612, -24021, -17229, -25833, 15206, -8725, 29307, 19409, -2505, -6800, -25166, 8761, 5982, 24878, 16616, 8235, -18754, -29294, 2730, -6807, 22727, -20524, -3080, -30171, -28184, -31209, 15174, 29500, -12426, -11865, 1687, 16191, 31657, -18904, -26751, -2576, -27389, 20810, 29103, 6420, -6410, -7633, 12256, 7460, -18741, -7936, -10155, -19954, -7425, -13317, -19452, -10949, 29405, 25908, 11537, -25060, 23407, -266, 16004, 3811, -14435, 2795, 22274, 1503, 4937, 29370, 21743, -27852, 32198, -18229, -5624, -31027, -8637, 31920, 3077, 6497, -7226, 2320, 4843, -2095, 8133, 21200, 22762, 12538, -13423, -5054, 26962, 15138, -15185, -27961, 9115, 1442, 31530, -23612, -10309, 4706, -9891, 7039, -20075, -24401, -2747, -9646, -25467, -7537, 18668, -16662, -19243, -3357, 13420, 2543, 15013, -489, -25296, 9718, 28344, -31059, -9962, 12582, 7415, -2970, 11239, 8717, 24910, -16148, -30134, -23168, 25571, -3874, 32691, 9138, 28773, 25990, 9439, 25705, -12625, -32108, -15710, 23545, 5654, 9704, -8054, 30529, 22110, 12510, 3800, 11533, -4484, -15412, -22659, 461, 26660, 23960, 16069, 17878, -22907, -26936, 24304, -19895, -4270, 26033, -16177, 9218, 31901, 14696, 8820, -385, -12831, -26219, -10257, -20375, -19419, 10729, -16889, 6886, 15039, -30371, 6201, 14810, -8815, -18487, 28782, -4212, 14382, 11009, -12592, 32330, -29995, 2628, 7270, 32564, 8513, -18963, -32658, -3320, -3331, 30453, -6473, -7208, -15983, -31712, -32757, 3336, -2351, 11978, 26568, -10001, 19879, 12177, 11408, 23003, -20408, -28455, 14834, -6630, 11082, 2222, -5776, 9328, 25278, -14320, -9406, -29322, -6154, 1946, 21066, -15220, -16635, 2989, -6636, -28281, 19905, 32732, 9578, 6017, -9473, -5486, -6503, 23253, -14429, 30015, -10101, 23436, 21152, -23617, -14877, 15830, 31324, 1977, -4072, 18664, 21269, 9864, 30915, -19191, 24202, 19178, -13138, 17916, -32091, -16834, -6619, -5864, -22420, -12650, 21484, 8634, -10444, -23667, -29181, 14288, 31295, -31207, 20777, -9919, -14935, -15371, -9510, 27721, -16069, -21072, -6672, -850, -8488, 8742, 31130, -16118, -10819, 9726, -13294, 12023, 30591, 19899, -4863, 12975, 30531, 8809, -20520, 2293, 20513, 17192, 7887, 16428, 293, -5688, -13146, 4409, 4178, 7068, -31336, -10307, -26781, 22429, 7211, 13038, 3828, -14064, 23212, -31941, -6694, 8285, 15506, -21837, 12824, -26357, 22303, 7845, 7028, 10507, 28961, 13807, -9088, -5956, 18274, -17496, -10227, 11617, -142, 29562, -14292, 17437, 11264, 28089, -21721, 28271, 7173, 11374, 13098, 13262, -28006, -18673, 7322, -12461, 979, 14726, 11070, -25772, 26186, -16320, -32205, -12795, -20045, -16434, 2216, 4690, -22860, 2033, 22397, -21474, -6341, -4859, 9988, -5448, -28463, -24695, -16183, 13173, 11772, 32508, -2399, -70, 25403, 26635, -26796, -9799, -13263, -27813, 11621, -18936, -9596, -613, 14570, 17485, 7131, 17562, -16058, -15342, 32151, 15968, 16353, -24463, 3207, -26329, 24242, -19669, 14346, 19656, 32239, -16780, -3050, -1151, 21458, 25964, 24334, -21724, -30191, 1760, 17549, -4639, 28656, -18405, 6997, -27071, 5642, -7514, -9757, 4788, 4033, -28208, -21728, -11294, -23379, 27265, 31395, 19561, 19068, 28553, 17248, 2253, -20088, -17614, 26977, 16719, 27827, -27143, -20125, -11779, 17215, 19950, 917, -12709, 292, -22371, 20516, -11948, 19690, -26419, -27695, 28859, -14585, 18033, -24782, -1105, 3088, 26254, 29662, 7811, 20279, 25750, 29530, 621, 893, 28582, -19666, -12557, 15270, 6953, -25056, 1108, -17456, 32629, 14232, -2372, 30852, 1422, 31783, 19843, -17251, -13053, -7544, -11913, 7978, -30204, 18934, 23305, 9804, 15308, 13986, -6923, 31582, -11087, -11337, -30748, -18025, -32584, 27893, -18300, 23008, -17573, 23238, -19580, 12956, -12155, -2693, -18179, -25274, 10934, 32676, -30299, -30097, 5410, 15958, 22704, -27416, -27868, 2139, 8245, 6603, 18096, -26653, 10157, 27480, -27352, -11215, -11508, 16761, 1825, 4386, 6687, -24801, -9884, -29250, 10308, -25355, 28874, -15621, -29299, 29287, -1478, -5674, 20115, -22865, -20549, -24160, 16820, -19084, -19757, -1849, -24341, 28268, 6584, 830, -23284, -28559, -14182, 20813, 19683, 20874, -1543, 6400, 3372, -15983, 10475, 6418, -5005, 17610, -23045, 29592, -8536, -13649, 29830, 5389, -19693, 4897, -4235, 15582, -23384, -18299, 25827, 9282, -1294, -10740, 13884, -5844, -14293, -11263, 28859, -24333, 29508, -22412, -19311, -20453, 6892, 18247, 24079, -5627, 5445, 10650, 4834, -6523, 20844, -29638, -16142, 23274, 17538, -4452, 17305, 14770, 2945, 31677, -27546, 31803, 5894, 31026, -4668, -23944, -32712, 867, 19945, -32453, -16708, 1954, 21650, 1184, -20099, -5788, 19532, 18868, -1619, 26952, -16365, 22589, 9308, -26171, 23772, 9414, 14256, 3104, -24163, -27278, -23534, 11061, 6250, 30854, 2801, 20079, -24307, 9017, 25189, -17112, 9053, 24502, 15466, 10494, -907, -1193, 31133, -14459, -17999, 6355, -20174, 31737, -9080, -27866, -17407, 21225, -7995, -15677, -740, 9830, -27697, -13973, 26841, 10494, 9353, -5198, -31484, 25099, -2535, 19338, -10235, -16118, 3050, 17137, -14076, 8821, -1959, 3623, 16576, -7529, 8269, 25560, -32008, 2390, 29942, -3095, -9910, 2452, -25587, 23509, -13101, -26498, -20874, -328, -3316, -27923, -28138, 1552, -3029, -1134, -12445, 2135, -13013, -3309, -6667, 15743, -30469, -25362, 26245, -22707, -24457, 3759, -609, 11572, 27284, -15426, 21171, 6889, -4484, 20273, -11000, 9579, -29952, 23362, 8067, -30678, 28249, -11136, -11505, -23398, -22008, 14590, 28869, 31043, -5123, -32211, 22547, -28112, 17399, 18250, -21653, -18849, -18006, 24475, -4259, 27543, 6599, -22157, -5754, -15582, 1492, 7812, -27127, -23199, -30043, -2653, 9753, 13287, -31949, 24995, 21733, 26401, 29874, -9135, -12667, -22862, 324, 27377, -11959, 10118, 29970, -16041, 7184, 22256, 28168, 4521, 18166, 810, 20398, 23497, 22643, 2310, 7123, 26850, 11720, 1222, -26099, 23558, 13211, 8748, 15862, -27434, 1716, -27786, -23936, -19437, -9901, -32725, 8004, -7307, 26262, -2032, 2260, -19655, 27178, -8249, 5318, -25442, -23788, -4330, -17990, 16865, -30165, -29346, 22048, -20520, -22851, 8559, -16401, 13512, 20989, 28837, -32733, 6582, 15543, 30140, 25940, -28113, 3507, 966, 10682, 9227, -12669, 3448, -31805, -11481, 17797, 18637, 1909, -28225, 18585, 29276, 19048, -5306, -26710, -12639, 17356, 2980, -8374, 29774, -20260, -27310, -13997, -14108, 5184, -15892, -12906, -32158, -19355, 14084, 12002, -31965, 30844, 897, 31705, -8579, -616, 3238, -15190, -10297, -22709, 13217, 17418, 3952, -13847, 9078, 3830, 27587, 11318, -13695, -26234, 6514, -15820, 11439, -1438, 24791, 23673, -20833, 31283, -32144, 6442, -21552, -25713, 18688, -17897, 13775, -27291, 4666, 14165, -29544, 8318, -16618, -3848, 27103, 14895, -7803, 4420, 13126, -420, 8430, 5724, 796, -736, -2757, -22947, -13839, -4130, -12677, -22732, -2660, 11477, 17506, -20428, -7106, 30527, -4390, -17488, -25892, 17525, 25932, 4506, 4697, -10622, -21841, 1271, 16580, -892, -10605, 27243, 5241, 22644, 30978, -8148, 12846, 5711, -30857, -11820, 11017, -6695, -4847, -12079, 16738, -20767, 4290, 23495, 19746, -20421, -15903, 24055, 6240, 21961, -30326, -23274, 19332, -13126, -25150, -9723, 9380, -23024, 15618, 5485, 14682, 11826, 7616, 5066, -26537, -24864, 30853, -3380, 4243, 54, -20820, 836, -26554, -809, -15427, -13650, -7611, 29487, 30635, -26166, 18875, -15009, 21627, 19909, -14978, -15461, -20711, -25080, -23067, 25717, 25296, -31193, 15860, -413, -17899, 24570, -14675, -14876, 11816, -18243, -18034, 4171, -7903, 19431, -14525, 13537, 7750, 24122, -18328, -25198, -26385, -4431, -12363, 17025, 29298, -18556, 30768, -10450, 32427, 8501, 276, 7526, -17106, 8773, -13132, -31406, 3078, 20735, 11120, 14759, 7064, -9298, 29838, 14889, 1083, 4105, -27029, -29943, -32617, -24237, 376, 9714, -12896, 8599, -31662, 5427, 3216, -18178, 27533, 21615, 22188, -20636, 26142, 27517, 31132, 13397, -1501, -4906, 30865, 15618, 22908, 7118, 17334, 22455, 22956, 6944, -32406, 18666, 2327, -8661, -28963, -17504, 14242, -29766, 11005, 3242, -7136, 20197, -4261, 6553, 9442, -6182, -22982, 5744, -575, -21653, -29763, -18908, 21075, 7092, -15248, 12617, -31041, 9379, 1827, -1428, -27730, -1804, 20985, -20144, -27412, 1971, -6310, -28293, -18501, -23173, 23645, -22730, 4273, 3358, 6278, 32093, -16249, -14096, 3518, -17064, -17567, 11870, -21571, 10230, -5933, 32342, -18965, -5539, -14641, 2387, 14216, -28541, -19584, -9805, 24931, -31843, 29440, -16951, 16853, 8809, -24181, 27393, 8533, -5959, 24713, -11977, -29944, 5764, -8814, 3201, 26719, 20844, 12039, -29657, -11562, 22167, 20361, 17015, 17765, -10748, -29754, -5338, 23690, 8314, -9650, 23353, -17942, 722, 8434, 6280, -1005, 18543, 3371, 32635, -16883, -1397, -20438, -10076, 16634, 22110, -7898, -21503, -792, -18271, -18084, -793, 15914, -20960, 6110, -16279, -15955, 15035, -19214, -1777, 31080, 26122, 31212, -23402, 25592, 21853, 26787, 28315, 20099, 17045, 15577, 28841, 22781, 15079, -21615, 23816, 3944, 7798, -4050, -32566, -28897, 9391, 7367, -8347, -8931, 28527, -7439, 17110, 7548, -14495, 15394, -22159, 29755, -20232, -31525, 15824, -6549, -9419, 4912, -18445, 32285, -28418, 17064, 17751, -24701, -21335, -16058, -27162, -7181, 9196, -17020, -12144, 7991, 27748, -26010, 32720, 2591, 8079, 12041, 13136, 29049, 488, 26684, -23750, 7224, -867, 28231, 7493, -15457, 29096, -11573, -19995, 8391, -21986, 19752, -22806, 18273, -6720, 23252, -32015, -16718, -31237, 21990, -27821, 4666, 20926, 12102, 17964, -712, -9109, 15747, 7807, -17810, 23725, -11550, -20560, 7668, 30593, 15114, -11249, -13843, -5563, -11262, 30725, 15736, -7785, 6548, -10526, -3257, -28628, 15541, -22451, -14995, -7168, 28240, 24712, 14856, 11172, 21589, 12197, 1987, 10208, -19551, -10190, 15063, -3572, 13112, -2009, -31781, 2278, 14854, 6076, 10548, -21069, 25085, -17367, 9339, -25753, 17879, -17114, 4184, 16886, -2529, -10167, -28552, -22789, 18781, -21642, -23336, 29050, 11569, 639, 9352, 19660, 20149, 19207, 30343, -11045, -27606, -21193, -32516, -9134, -2219, 19964, 4166, -15779, -1658, 4894, -18377, 23875, 2766, 27320, -21252, -25173, 26946, -7178, -23258, -13752, 6052, -517, -9110, 21278, -25185, -30192, 27275, -23987, -17418, 25938, 18989, -14903, -10125, -22572, -25272, 1815, 5172, 8555, 7667, 12455, -23336, 21689, 23444, -1509, 31606, 30747, 4708, -21802, -18716, 15972, 14706, -22046, -15754, -22686, 28137, -14676, 18893, -13479, 23913, 23705, -18105, 17614, -21282, 2065, 29026, -15261, 18546, -23014, -14857, 9912, -8323, 31472, -25802, 23705, 28643, -22482, 20008, 20247, 13997, -22760, 21904, 11668, -17842, 19894, -10681, 300, 32105, 29662, 17183, -191, -322, 28659, 7027, -17112, -1938, 18363, -21589, -8527, -9698, 21058, -6919, 32379, 4886, -770, -11082, -32552, 5400, 12148, -20582, 30057, -16458, -31045, 26634, -22834, -21644, 6998, -14692, 13261, 23120, -8356, -2889, 4774, -11810, -29916, 20086, 990, 2449, 2723, 24327, 20289, 14470, -26500, -8189, 8080, -12053, -1853, 22752, 12885, 14537, -1000, -17635, 3415, 9977, -13458, -31646, -28246, 27139, -1410, -27471, 2257, -20735, -2589, 12250, 31062, 1716, 28438, 4149, 5784, -9004, 21410, 22728, -9685, -24500, 13720, 13212, 2956, 19954, 9839, 8898, 21729, -1329, -11327, 6374, -4414, 30843, -17451, 5376, -17583, -23032, -23003, -20367, 8089, 24884, -179, 11019, 6207, -27618, -6837, -7765, -23385, 24960, -31058, -10555, -16762, 15744, 8781, -19700, 17648, -4700, 20230, -32447, -17913, -355, -27217, -4672, 21187, -19770, -19769, -4220, 30464, -6916, -32237, -19858, 28635, 27120, -3992, -31891, 10738, 16240, -4651, 20491, 14256, -7857, -3180, -17952, -24868, -27502, 19024, 26009, 30458, -16681, -23734, 18656, -369, 5805, -25299, 10043, -7900, 17189, 12169, 27780, -25848, 30719, -32066, -9905, -21787, -29417, 16978, -19717, -16960, -7630, 8867, 20523, 31195, 26475, 4891, -12323, -7794, 27529, -1601, -25043, -6221, 6004, -13816, 23944, 23096, 23953, -29794, 26554, 27910, 28118, -26143, -24941, 1007, -19147, -8773, 9734, 13796, 9867, -1917, -6169, -30680, 6394, 6257, -7207, 3755, -10001, -25971, -4073, -25748, 6419, 16649, -6718, 31350, -20796, -27745, 2367, -10343, -18961, 14679, 11400, 9951, -15517, 29275, 13075, 25913, -18184, -26475, -1094, -5048, -11921, 594, 21860, 2250, 32532, -3191, -29882, 22171, 3480, 12904, 992, -32157, -11506, 20204, -922, -20442, 23112, -28793, -28558, 25565, 18454, -14543, -513, 20489, -19994, -10185, 25308, -20081, -6995, 6555, -26967, 18114, 29239, 19854, 6035, -30412, -27817, 31077, -18684, -5345, 3828, 20188, 19255, -8430, -14105, 14291, 30705, 3884, -6723, 29888, 14833, 20720, -13173, 13009, 5409, -11410, 31792, 7095, 24614, 26621, 28660, -28829, -2937, -1796, 11696, 14657, 14819, -26876, 25713, 31126, -32190, -8475, -8110, 7415, -23687, 24843, -22308, -12895, 18742, 983, -8792, -18650, -26534, 20268, 15095, 3944, 26705, -11534, -6069, 28523, 9534, 2801, -1752, -14228, -28037, -24704, -3922, 6764, -15426, 13505, -26006, -26008, 18599, -7425, -3768, 28239, 25549, -2670, -7959, -8132, 13569, 3024, 16284, 23416, -19550, 22348, -14323, 22637, -9719, -27161, -1443, -3256, 14325, 22071, -9014, 28092, -4286, 22257, -18435, 16593, 21912, 4101, 25659, 31539, -26058, 2856, -4594, -30489, 2736, -26511, 17787, 30620, 18439, 8173, -19133, -13500, 16619, -27976, 26310, 20135, -8328, 5516, 2924, 24270, 7880, -26192, 8803, -21151, -6850, -23045, -5191, 28023, 30033, -29232, 11959, 9300, 14188, 2202, -10795, -24461, 25258, 31600, 20158, -7691, 1205, 28388, 13149, -14526, 8712, -22053, 27721, -3437, -9580, 5127, 31723, 28514, 11145, -22865, 12407, 31701, 13623, -7343, 5822, -29835, -25277, 24879, 923, 3752, 15757, 28725, 17915, -23665, -13835, 22341, 25003, 29696, 1484, -5931, 36, -25170, -25389, -30883, -15485, -15661, 11365, -4452, 28900, -32465, -9414, 462, 24480, 7682, 20646, 4185, 11559, 22236, -8522, 13154, -2590, 8622, 9574, 16827, 4396, 2777, -9381, 2383, 26020, 22090, 7109, 11225, 13580, 27119, 30362, 29606, 7663, 21733, 11551, 29639, -30035, 22912, 5373, 1452, -30443, -1546, 22609, 29648, -8031, 26440, 14173, 23323, 7991, -6840, -26887, 18290, -7058, 28391, 9969, -5366, -8013, 12534, 1849, -9766, 28465, -8914, 2351, -13525, 19053, -32073, 22387, 21989, -18676, 2498, 24015, -18304, 4157, 12834, 32106, -28670, -32178, -16651, 32733, 10223, -5267, 29473, -11220, 4900, -20108, -22654, 11801, -12579, 23011, 31569, -29740, 10538, 22432, 10504, -25633, -12941, 26609, -24138, -19667, -2173, -15102, 12367, -1164, 19846, 9779, -3231, 26675, 22194, -12253, -10173, 12986, 14145, -5772, 12975, -26973, -20372, -333, 24209, -26685, 1032, -10063, -13300, -27952, 31950, 20363, -27072, 32557, -1306, 26565, 27430, 29001, -25726, -12646, -26957, -14913, -941, -10706, -22073, -26616, 28025, -18294, -15149, 9584, -24295, -9435, 30242, -3592, 8802, 22028, 3251, -2694, -30912, 21039, 4816, -20486, -909, -11625, 10565, 29370, -27061, -326, 5251, 32092, -1937, -3833, -31222, 22727, 21107, -24454, 21103, -32122, 8787, 13307, 11537, -26433, 15130, 14713, 20351, 17362, -2483, 22166, 1147, -12645, 4152, 1761, 11976, 31274, 11584, -18667, 32238, 981, -18822, 2634, -2488, 17135, 28289, -13902, -10723, 26551, -11487, 23479, 12730, -9931, -22221, -13444, -4238, 27574, -25267, -15277, 11816, -31929, -13173, 20805, -25235, -18552, -9154, 32559, -26130, 11248, -18645, -17555, -30619, -12895, 9922, -8350, 26036, 31676, 9435, 26594, -30617, 31930, 17087, -32373, -26851, 27850, 4645, 9213, 22603, 21150, 317, -395, -29342, -13980, -3698, 4439, 10191, -19756, -31184, 15660, 5086, 27103, 16653, 9864, -28201, 10229, -11470, -28541, -24107, -30321, -25219, -18355, 14720, -7884, 21779, -21849, 14134, -22100, 6808, -14991, -14315, -26145, 22669, -4616, 10417, 16536, 31824, -21250, 4465, -14605, -12103, -10422, -22735, -4066, -28850, 18732, -26973, -1076, 20270, 4325, -2259, 20590, 20042, 27886, 29375, 20898, 17158, -9232, 32102, 21420, 22749, -12704, -4019, 13538, 3921, 5494, -22951, -815, 28280, 10142, -14542, 5070, -32568, -197, -9694, 27618, -3573, 2644, 17220, -3017, 3465, -2144, 32673, 25881, -5261, -6626, -10522, -8554, 11309, 30308, 9148, 24636, 32508, 20185, 18987, 11251, 23636, 28891, -28187, -31693, -15186, 5401, -10718, 31389, 29576, 15668, 23822, 14883, -6326, -32286, -6348, -8554, 27746, 12095, -16980, -8573, 24848, -2329, -3111, -17971, -10639, 18812, 29202, -21265, -3043, -8384, -5939, 18956, -22695, -16541, 11548, -8414, 16900, -13249, 477, -2996, -32099, 24915, -2343, -9410, 24346, -20731, -31135, 30983, 9767, -20315, 13139, -20081, 15224, -14886, -32405, 25866, -29044, 14764, 28273, 3285, -32333, 31748, 19870, -684, 1188, -32597, -126, -7361, 28619, 14599, -11496, -29465, 20018, -4078, -3703, 1898, -3703, 6732, -573, -11740, -30383, 11519, -2445, -19778, 2368, 1254, 1494, -6345, -23495, -5682, 1101, 11109, -1472, 8159, 8863, 3035, -8303, -6591, -23182, -21299, -5141, 21960, -24305, -1173, 3138, -8608, 25113, -12492, -12453, 28245, -23067, 38, -26564, -15351, -32615, -13638, 6176, -11403, 26612, 26936, -9412, 13122, 26978, 25967, 8502, -10779, 32243, -24844, -3149, 23034, 19719, 13652, 26464, -22615, -27697, -16321, 27091, 25442, 553, 2446, 5101, -26176, 7085, 9734, 4, 26170, -27037, -27384, 32243, 30343, 21919, 18372, 3918, 16599, -28077, 31176, 13691, 19318, 2084, -15212, -19756, 8570, 13119, -23790, 30801, -27584, 3301, -13460, 8049, 12323, 19891, 32312, 18301, 13642, -17772, 14176, -18202, -19251, 3760, 21004, 6169, 5153, -15975, 9208, 29123, -12999, 7291, -24520, 16225, 24968, -21886, -14312, 25316, 28714, 17893, 16888, 1184, 4573, -9555, -1651, 19078, 24343, 21293, -26811, 5137, -21191, 32077, 14374, 29042, 793, 24272, 28185, 28022, -12267, 19355, -14209, 623, 2456, -17520, 9682, 28195, -12520, -4851, 17109, -7934, 28210, 24362, 32449, -31519, 32400, -24588, 8537, 18220, -8381, -32188, -14789, -23069, -26903, 12004, -11441, 17789, -13882, 31508, -31647, -23823, 9612, -14897, 11474, -10646, -1725, 9576, -30484, -27291, -19981, -18159, -9301, -27259, -16802, -8162, 4819, 18917, -25926, -20839, 21296, -18604, -17590, -23384, 19040, 6929, -26871, -28169, -18466, 476, -475, 17528, 20623, -18552, 26150, -18105, 9028, -489, 30986, -3253, -1654, 833, -4723, 17525, -2559, 3591, 23601, 28628, 8276, -4451, -28407, 31027, 29058, -12400, 15096, 10852, -2349, -1626, 19348, 19764, -32518, -11582, 17214, 13002, -27903, 5704, -25245, 13168, -5204, 31716, 8709, 10624, -501, -24470, -28905, 9894, 5832, -24288, 781, 21416, -31737, -12210, 6998, -2177, -21844, 21481, 25040, 27364, -13282, -14807, -17445, 28588, -21421, -13049, 17749, 2249, 16197, -27387, 11600, -9468, 654, -28211, 14605, 30701, 25808, -7689, -13681, 4774, 26447, -19691, 3483, 30443, 26720, 14035, 29449, -31719, -10592, -12265, 9952, -10306, 6466, -28540, 209, -7811, 4255, -28349, -7178, -12551, -10330, 23569, 25227, -3450, -16862, 32678, -23454, -8755, 8175, 21533, 11618, 15867, -14047, 15821, -2517, 19390, 27624, 32000, -3416, -21517, -32443, 20976, 6422, 25305, 3558, -16386, -15797, -20837, 10185, 8441, -10022, 24534, 27057, 9700, -17374, -12411, -15162, -502, -28918, 8947, -1062, 6229, 20095, -31001, -6160, -16632, 8196, -17033, -8810, 20046, -423, -6287, 20133, 24932, -30778, -22422, 15347, 3526, 22029, 3348, 17566, 19712, -22878, -24220, 28037, -1641, 16108, 28456, -3644, 22499, -19422, 31080, -2644, 26252, -15023, -11154, 23425, -7923, -6699, -20930, 7446, -32326, 27885, -10751, -3369, -29814, -19024, 30579, -31083, 26499, -2864, -9362, 18989, -6314, -19977, 11925, 12696, -7660, 28726, -3292, 26961, 32330, -18273, 23628, -8575, -31657, 23659, 31830, 10569, -30063, -801, 4390, 22672, 9369, 10127, 3222, 3845, -22501, -14546, 15383, -21454, 8124, -22457, 1985, 5504, 799, 27043, -23363, 13962, -4663, -23426, -30104, 827, -4088, -4899, -4406, 22677, -12377, 14002, -27436, -11829, -5159, -28602, 25405, 28358, -2379, -15083, 14988, 2826, 19092, 6457, 4316, -4678, -29078, -22616, -3902, -14986, -6972, 3800, 28712, 19983, -19704, 30950, 29858, 3797, 24816, -22620, -32704, 26758, 11237, -14042, 19324, -32439, 28772, 30693, 22866, -14066, -21222, 19314, 9605, -12743, -27094, 19180, 1499, 18190, 15149, -24078, 14819, -16282, 29703, 26595, 22673, 19430, 25066, 4164, -28706, -27156, -23581, 25235, -1675, 31714, -4748, -25194, -4528, 4810, 16514, 22389, 3269, -2533, 19682, -17563, 25502, -3252, 10263, 5295, 31114, 6804, 21230, -6717, 30911, -30991, -12368, -2787, 28419, 12728, 19530, 7493, 9105, 25534, -12079, -8691, 22513, -8784, -1808, -10873, 23186, 13154, 31386, -23083, -15539, -15730, -7445, -16230, -31083, 30647, -27324, -18304, 6279, -1474, 27428, -31658, 22189, -17984, -1513, 3275, 26351, -23903, -3399, 16479, -18483, -25604, -1676, 15061, -5650, 18970, 12327, 13321, 17506, 9858, 29289, -17532, 28124, 26267, 23158, -15716, -16889, 15884, -27409, -20025, -1466, -31306, 8614, 32493, -653, 23260, -11311, -18641, 17578, -10636, 12995, 1566, 19667, -11185, 22550, 22973, 7278, 32725, 23695, 1779, -15910, 25345, 3818, -7782, -19087, 23746, -3019, 23837, 30077, -9576, -5360, -14477, -7739, -17863, 30396, 25812, -9346, -2157, 10095, -32472, -7148, 30859, 21477, 24679, 7553, -10548, -4522, 12320, -16910, -24622, -2228, -20374, 29, 2063, -23838, 18909, -17788, 17610, 18394, -9183, 26629, 32177, -20361, 31057, -17182, -2230, -17749, -14483, -6915, 12176, -3687, 20155, -17657, 8133, -6564, 4259, 3571, 32421, -7953, 11688, 18622, 8461, -31886, 1841, -9653, -32327, -3635, -11621, 24429, -32005, -26877, -4207, -9081, 20187, 9020, 25489, 32740, 12352, 11778, 8545, -12013, -30599, -22299, -18699, -11286, -16787, 25263, -29536, 27054, 16407, -27214, 32433, -12402, 9212, 12659, 1094, 16675, 15362, 30826, 15964, -18695, -985, -32564, -5276, 5313, 18082, 24690, 32004, 29496, 1592, -12293, -7294, -17142, -11402, 32018, -30927, -6423, -15528, 86, -4865, -28856, -14853, 2433, -4417, 19266, 7192, -21971, 10922, -21958, -1923, -6945, 11149, 6598, 27914, -1185, -6989, -25414, 5454, -28031, 25474, -20033, -12859, -19065, -18574, 4527, -9212, 807, 31754, -26129, -14595, -10079, -32730, -28144, -20365, 26243, 2450, 8706, -23192, 26587, 25908, -6607, 5697, -22545, -2866, -12037, 20747, 14380, -18375, 14973, -22921, 19006, -30633, 9584, 7219, 29678, -21828, 14068, 11109, 5419, 16157, 27070, -19819, -642, 28980, -20621, -20852, -15678, 28614, 29192, -23077, 7517, 18929, -32305, -810, 1973, 14671, -16585, -8998, -19904, -19816, -9817, 26329, -13068, 20534, -5504, 29613, 26776, 16511, 18493, 28633, -29517, -4735, 20961, -28360, -32706, -16496, 7493, -3843, 31292, 11451, 1893, -17203, -26921, 24494, 25120, 31128, -13433, -14968, -3706, -32132, -16806, 15552, 31680, 20007, -25959, -29659, 17007, 10084, -6425, 10199, -25722, 10168, -5304, -10870, 23130, -20215, -11120, 20833, -24417, -1833, -14056, 22541, -22351, 15883, 32118, 27681, -2310, -31444, -4358, -23379, 10049, 29130, -32759, 28951, 6241, 15453, 23055, -3982, -14012, 13967, -1386, 5823, -30176, -20058, 10143, -17040, -15772, 10165, -28022, -16435, 714, -1670, 11664, 13486, 10991, -14419, 17019, -31069, -29985, 17841, -4846, 5049, 26346, -13176, -15692, -31223, 9738, -6104, -19281, 13801, 18822, -16226, -14632, 6950, 4993, 18249, -10790, 5561, -18590, 32613, 30132, 16816, 26406, -23008, 6175, 22850, 4049, -22171, 18150, -16721, -15217, 24909, 27145, 28252, 12278, 11883, -18017, -3963, 3257, -19018, -18736, -32220, 26571, -15168, -4531, -11264, -2298, -5206, 5575, -15390, -22014, -13768, -2109, 10390, 8966, 20825, 31417, -11100, -22623, 27860, 27073, -15791, 9264, -16377, 9609, 15830, -10887, 18254, -10834, -9012, -6896, -16628, 6722, -29888, 24781, -16397, 18480, -13928, -5527, 727, -22378, -15845, 18303, 20667, 30554, 3748, 13762, -20102, 19949, -25813, -3386, -10187, 8113, -19173, -12620, 20723, -5023, -18427, 15931, 5811, -22995, 11382, -26326, 1761, 12320, 29959, 15318, -1481, 16361, -8618, 632, -14256, -9791, 9329, -29889, 28438, -14617, 13239, -5268, -4732, 1205, 287, 26719, 27258, -14613, 12933, 3070, 2679, 28691, -13843, -20704, 6271, 19237, -1801, -23049, -11531, 10865, 17924, 6061, 5150, 32003, -17025, -32741, -28397, -14023, 813, -8320, 26342, 4217, 28287, -31815, 12864, 9056, 257, 11854, -21664, 24659, 28782, -29154, 16267, 27863, -12093, -25978, -4841, -2887, -3632, 1843, -14224, 19113, -27843, 22794, -20931, 28517, -23872, 18632, 23296, 19595, 12717, 23708, -23397, -29957, -14667, -3088, -4311, 19128, -15069, 3583, -10588, -27964, -14277, 8749, 22750, -26626, -28249, -16897, -8863, -30545, 20493, 6841, 15904, 4644, -17467, 30167, 1963, -7430, -14180, -21052, 17139, 2129, -32515, 2454, 19843, -6350, 22305, 30854, -15045, -15924, -16884, -11481, -5179, -32636, 29998, -25821, 271, -18594, 1083, 13945, -8942, -8240, -23532, -2436, 5084, -13516, 15916, -27253, -4397, 8166, -21350, 5051, -8225, -22738, 27122, -8185, 8079, 12748, -10670, -26513, -21808, 14727, -15709, 5071, -10154, -13232, -15063, 2556, -24750, 27139, -7611, 12303, -25207, 7406, 17862, -5009, -2917, -28263, -28922, -8867, -21446, -28073, 13681, 15057, 1692, -9684, -2777, 23766, -5649, -30264, -9524, -21578, -28613, 11026, -13391, -29369, 19360, 22045, -5691, 8706, 30616, 26068, -25395, -16342, -6226, 7308, 2406, -22603, -21420, 25011, 4720, 27582, -3440, -16392, 13287, 22717, 675, -20811, 7794, 5081, 9809, -16066, -7261, 32063, -19199, 15030, 6184, -2179, 26037, 26679, 14550, 11947, 23959, 4940, -28231, 31960, -24300, -25236, -75, -8262, 8092, 24731, 22749, 19585, -19279, 26313, -12708, 4396, -28785, 29284, -17475, -9047, -13899, 14898, 20740, 29822, -19651, -8284, 32244, 5999, 31970, 31672, -30971, -10086, -977, -1919, -7024, -29132, -15164, 16422, 26784, -3910, -14390, -8166, 17419, 24213, 32286, 1864, 4601, -14078, 8353, 26894, 1503, 25351, 4179, -30112, 18732, -4995, 30469, -31730, -19484, -14444, 3104, -24129, -24053, 10771, -10805, 12196, 18436, 4804, 19837, 30742, 7864, 29, 13330, -27307, 12667, -14054, -25113, 26209, -24002, -31137, -3545, -29726, 12412, -16517, -11056, -1721, 27134, -5579, 5578, -1017, 423, -25339, 13697, -17127, 31034, -7270, 28921, 22685, 2857, -25396, -21083, -25958, 18375, -16225, -12872, 17458, 16193, 18130, -19419, 18427, -32416, -7275, 6262, -3647, -6160, -234, 30672, -22565, -14068, 26856, -10306, 21998, -27999, 28643, -26149, -5817, 9535, -11337, 26418, -31676, 3025, 17889, -15639, -13306, -10106, -29347, 28368, -15243, 27747, 31012, -22046, 15111, 3809, 10299, 18814, 22123, 31566, -18328, 29338, -8878, -18356, 7344, -26176, 20301, -13847, -24698, 13244, 24677, -26335, -28756, 8892, -3875, -32228, 4850, -12961, -23640, 20263, -15771, 28568, 20375, 18286, -521, 8205, -835, 4532, 4804, -10614, -31152, 10792, -1777, 12403, -8022, -20352, 667, 17044, 1621, -29419, -9280, -29794, 18240, 19655, -22669, -27419, -11976, 7166, 7046, 1684, -25729, -9823, 24152, 23727, 1718, 15508, -31443, -28993, -466, 27031, -1152, 25904, -24040, 9495, -12629, 16468, 1424, 25565, 16427, 7686, 3846, -20825, -17187, 21474, -2159, -28573, 15870, -29520, -8105, 26527, 30374, 6738, 13215, 24371, -24603, -15753, -32124, 20159, -213, -6185, 2447, -15355, 11221, -1877, -30722, -2443, 20196, 30782, -7595, -9565, 2890, -24221, 22208, 8304, -12573, 28688, 487, 24027, -21008, 12999, 27562, 13838, -771, -9100, 1405, -1954, 7961, 24601, 14577, 22955, 19801, 25088, -20615, 8287, -8795, 31513, -2466, 5238, 9401, 5751, -28686, 31579, 9562, -4067, 826, 2271, 32099, 30632, 26507, 9472, 9437, -22320, -128, -18047, 4045, -12465, 10384, 566, 14455, 31368, -5249, -22683, 31986, 26324, 15358, -19128, -11812, 27695, -11104, 12052, 30001, -32263, 13245, -3927, 11272, -22709, 19168, 27840, 13759, -24472, -23558, -13459, 1550, -4509, -20355, 26068, -7926, 15692, 5504, 6241, -22700, 5367, 28290, 10114, 15899, 26036, 9169, 32519, 27487, 23905, -1487, 2437, -9361, 31520, 18285, 22874, -25061, 24846, 21545, 19239, 4641, -30564, -15867, -2720, 11599, -26089, -23454, 7953, 593, -19796, -15736, 30490, -1913, 18702, 31084, 21238, 16989, 14065, 7876, 7226, 9603, -32428, 10363, 14323, -25665, 25101, 508, -12838, 31465, -7933, -16420, 6962, 31393, 19830, 12029, 30565, -14756, 15288, -11755, 700, -19082, -29837, 8522, 9539, 25431, 776, -5470, -13381, 11146, -24375, -18570, -9543, 13891, -7918, -6277, 27194, -20794, -1491, -12781, -17929, 166, 14667, 29558, 5652, 27925, -10275, -595, 24418, -4528, 1350, 22849, -12897, 20155, -19900, -17141, -24986, -13848, -11350, -8601, 27368, -17771, 2050, 31257, 5446, -19469, 16827, -428, 432, 26742, -4369, -15412, -25705, 27337, 15625, 7384, 10159, 8196, -14801, 3116, 13624, -15777, -14100, 29727, 20772, 20333, 20646, 24712, 28808, 18675, -31651, 4947, -6765, -27919, -23957, -11589, 20417, 3749, 8518, 26337, -29978, -10033, -21728, 9255, -24470, -26923, 5440, -22405, 10444, 15579, -23769, -26606, -16553, 12047, 24781, 11976, -17312, 4885, -5632, -27798, -15818, -22249, 29264, 14621, 21736, -22597, -22944, -16672, 23525, -7427, 17788, -22605, 20815, -3107, -22137, -12597, -13198, 17763, 22158, 4923, 2134, 14087, 2577, -11422, -29381, 23824, 30744, 8981, 3241, 4046, 32584, -15805, -11296, -13425, 26605, -22636, -13850, -11909, 27438, 13599, 8160, 495, -18288, -29075, 4494, 19677, 16987, 734, 21061, -12494, 23898, 24835, -19512, 6573, -30058, -1736, -3472, -8871, 14842, -25712, 10184, 30627, -813, -14626, -11089, 1571, 27494, -18057, -24711, -19178, -15530, -28475, -21109, -20152, 6192, -13665, -7376, -16965, 20052, -30258, -12619, 31298, 5457, -15905, 6178, 22871, -24049, 31851, -24579, 12913, 6028, 2536, -25930, -8889, -22556, -27570, 26638, -20718, -12912, 6087, -9745, 6361, -9635, 10468, 19961, 8644, 11935, 12929, 23958, -30963, 14092, 20756, 13701, 24732, -27272, 17531, 9282, -20498, 31716, -13190, -29228, -7056, -22220, 13148, -26002, -13582, -7105, 29875, -15017, 26893, -18383, -21679, -308, 582, 21120, 14310, 2968, 26241, -19273, -29474, -18759, 22845, 17007, 17257, 19323, -21548, 17331, -15430, -5690, 4675, -13337, 11984, 25359, 18169, 3040, 25829, -9498, 7141, -14371, 19210, 4794, -10854, 26189, -30096, 18472, -9907, 12725, 16962, -32586, 28182, 10908, 26690, -30669, 31236, -1772, 21513, -24508, -17057, -18030, 11188, -7798, 13163, -19179, 16094, -5836, -1193, 1108, -32582, 24153, 19971, 15721, 5487, -12171, -14579, -27700, -12053, -7286, 26373, 27225, -12368, -21147, 19289, 605, 2456, 9777, 3131, -8009, -6230, 8797, -66, 18772, 27458, -21953, 18488, 4274, -19097, -25169, 25714, 20791, -2090, 17150, 21238, 20173, 31588, 30909, -8878, -16162, -8374, -20723, 17369, 15548, -13377, 30365, 9752, 10124, 10551, 11842, 5840, -23809, -12719, -12814, 17726, 18418, -12123, 12586, -23757, 29273, 7769, 25469, 26894, 9547, -28436, 15141, 8774, -9874, 32364, 20168, -7751, 13522, 9329, 16641, 21407, -23067, -24382, 4653, -4279, 30053, 28921, 5334, 32689, -20737, 26841, 24542, 29311, -5805, -4112, -28169, 23938, 22998, -22799, -11756, -20668, -30666, -14774, 24826, -19633, 30737, 914, -10578, -18606, -164, 24690, 18289, 21828, 383, -18609, 16091, -8374, -24117, -18986, -22181, 16242, -2046, 12786, -1248, 5551, 25538, -32158, -13695, -7047, 26303, -27790, -9438, 16874, 166, -7643, -22788, 15263, -2131, -25693, -17835, -26880, -21954, 4375, -12774, -28334, 31364, -8239, -705, 10763, -15191, -17616, -18006, 13301, -25793, -5826, 27488, 8072, -13326, -4230, 32530, -11601, 28707, -23291, 4870, -985, 20394, 16170, 17002, -30499, 28701, 3172, -14328, 30000, -11374, 13795, 31673, -23488, -19228, -20663, 26149, -6497, -11301, 8054, 3008, -17415, -6637, -1250, -8273, 27511, 13208, -26179, 8429, 7046, 17108, -15153, 24699, -12788, -20012, -16672, -30956, -5162, -20513, -13065, -24774, -10530, 20706, 10755, 3190, 15562, -24054, -8267, 2202, 12169, -20141, 19453, -9934, -28483, -20472, -10412, -7386, -20846, 11757, 21037, 17543, -3097, -29396, -16107, -4870, 20343, 13472, -25928, 13003, -11924, -26461, 12419, 2173, -26941, -18886, 12849, 14316, 9023, -18720, 18736, 31310, 19158, -20793, 14217, -2548, 30821, 10211, 6671, -25830, 1712, -27437, 32640, -12765, -23543, 15811, 22971, -22799, -28875, -29829, 23011, 7535, -20378, -8773, -5439, 22076, 6417, 19131, -13345, 10336, 27023, -9802, -23621, 20395, -9825, 4502, 17460, -23468, 24857, 17946, 23941, 4644, 3769, 24119, 13418, -10763, -12399, 16455, 10389, -25485, 9910, 6756, -407, -16747, -32334, -26174, 24904, 7323, -8842, -28163, 4107, 15815, 13874, -12345, -6981, -15498, -10259, -18685, 8685, 18100, 19132, -7944, -13657, 21247, -1239, -5233, 19178, -14508, -1617, -6581, 13190, 8976, 19631, -26306, 24509, -31815, 10637, 29934, -25950, 861, -13781, -3114, 12758, 18475, -12683, -5772, -21559, 18055, 10756, -599, 4377, 23422, 26721, -21833, 8808, -29807, 2312, -5593, 2693, -22666, -5735, 31251, 4395, 23803, 31043, 23561, -11549, 4891, 1052, 7600, -31284, 13267, -30402, -16692, -29612, 16095, -389, -14376, 23088, -5091, -2159, 32429, 31854, 31758, 24640, -16987, -32619, 26300, -25243, 12762, -21679, -17443, 1597, -29739, -8895, 29451, 3726, -19651, -4919, -6918, 23967, -10429, 22952, -16025, -7187, 10481, 3910, -6723, 97, -32296, -1274, 16302, -6621, 16120, -26914, -14044, -11933, 28133, 11824, 14596, -13747, 23255, 1245, 2237, -4026, -6347, -22290, -21511, 1736, -18544, 22067, 3460, -16969, -8968, -7117, 3676, 4033, -27894, 22943, 21899, 30448, 18656, -1546, -9111, 26550, 22312, 13779, -2343, 10822, -1555, 20271, -26673, -20001, -31580, 28783, 17201, 3205, 20381, 25891, 16729, 818, -3319, -7743, -20358, -29573, -20690, 3674, 27075, 19866, 9060, -31480, -6189, -2430, -25612, -6621, -20409, 19263, 7609, -8852, 24305, -11904, 8520, -16080, 6682, 18245, 31638, 10843, -1584, -19120, 3782, -2959, -20650, 16887, -19375, -7926, 11422, -2507, 26105, 15736, 13950, 17726, -26214, 6464, 23956, -16350, 2557, -11338, -28731, -11172, 6923, 16696, -28484, -15131, 27615, 31350, 13281, 22052, -25790, 27757, 3775, -17695, 28613, -18334, -17679, -1922, -26375, -1428, -4937, -4684, -13076, 30141, 22645, 2700, 22359, -8987, -747, -25323, -23595, -1384, -23433, -27117, -5355, 20383, 22549, 19201, -28288, 26355, 15514, -24011, 13165, -1276, 29895, 12314, 10756, -19619, 13852, -16628, 20543, -12084, -30907, 3666, 127, -6155, -18104, 8872, -4397, -21839, 32304, -1315, 9319, 22125, -6064, 14439, -1829, 10055, 25607, -29381, 5777, -29138, -6863, 3349, -5984, -32730, 17571, -4640, 6722, 17901, -27056, -26410, 7395, 3191, -27389, -12173, 22772, 1997, 26639, -27678, -24490, -7024, 16984, 29355, -11604, -2780, -24572, -26615, 20777, -24704, 27820, -29382, 27141, 22721, 12992, -1695, -21102, -3941, 12708, -15452, 17399, -30505, 24545, -21265, -8620, 26531, -25097, 18384, 20244, 23482, 16416, 457, 26482, 17063, 25933, -32681, -7406, 19375, -29377, 112, 8590, -1616, 28897, -6940, 2291, -29874, 2718, 23248, 4124, 29188, 4858, 18982, 17851, -23335, 18305, 31771, 16398, -10739, -25522, 10063, -10694, -6567, -11523, 14518, 32568, -23446, -3878, -9351, -19094, 15420, 16775, 8564, 7977, 23521, 20832, -6242, 3100, -23925, 4784, 25284, 71, -13747, 29565, 25756, -27049, 17926, -22512, -11595, 22684, 24044, -26170, -28538, -5791, 30387, -25318, 23936, -21457, -17886, 17322, -11511, -8104, -990, 16638, 8833, -19859, -31924, -18200, -2353, 15777, 19543, -29981, 21187, 15259, 15906, 30803, 26273, -385, -22237, -6437, 26942, 17484, -15171, -1695, -9995, 32247, -26732, 784, -2337, -23420, -12045, 21464, 8702, 29911, 11714, 5967, 4221, -19542, 23183, -15081, -16965, -18036, -3534, 16018, -3309, -8056, 23936, -21929, -5210, 4584, -30340, -8086, -10774, -21478, 6917, -23509, -14212, -27499, -18773, 4164, -19011, 15180, 31561, 18779, 22294, 5075, -18324, 20124, -30907, -17285, -24844, 18328, -31829, -2731, 11740, 22514, -16603, -10029, -10318, 510, 32563, 23437, 2434, -32567, 31958, 21322, -10612, -4613, -8420, 859, -1736, -15279, -16637, 14031, 3791, 31331, -2034, -11313, 21266, -31715, -23289, 10325, -9726, -12476, 13938, 29476, -22185, 17533, -20914, -13553, 5354, 26058, -3460, -11216, 6367, 23034, 7689, 29733, -26142, -15379, 9483, -3571, 25635, 16933, 6768, 6598, 29896, -30112, 26698, -11435, 3952, -18190, -5751, -12568, 5844, -12596, 21412, 24789, -14369, 5694, 5717, 975, 9837, -24054, -19918, -8024, 17100, -26466, 4111, -18120, -20163, 1004, 14699, 27107, -23268, 28774, 13125, 16127, 29089, 24051, 23333, -26216, -25582, -20297, -17862, 6281, -19921, -10482, -9048, -6255, 29131, 22233, -13056, 1698, 4998, -26896, -27188, 5763, -6333, -10397, -14062, 16172, 19414, -19776, 10062, -732, 26331, 28515, 18087, 17848, 23637, -2456, 6011, 25952, -19044, -26451, -21399, 3471, -21833, 18111, 1950, 6256, -20963, 21962, -4623, -12338, 4447, 12855, 2480, 11672, 14553, -32443, -15576, 28464, 32474, -30690, -25589, -20827, 6496, 6879, -32747, 32703, -10227, 25872, 12778, -30447, -13626, -687, 413, 14392, 6816, 15542, -23951, -10434, 14640, 31613, -333, 10716, -17883, -32586, 22549, 4482, 11946, 4028, -21983, -6435, 7665, -6530, 23710, 7824, 32590, 14848, -17393, 4505, -28586, 25668, 12086, 8524, 31078, -31023, -20184, 3270, -17895, -30798, 10949, 1013, -10573, 28033, 30725, -18414, 25249, -12127, 8165, -15585, -28309, -15011, 8223, 20069, 7739, 28540, 12662, -1245, 3460, -17302, -9023, -30281, -27789, 2626, 26256, 6943, -11951, -23032, -28248, 33, -31744, 9996, 15377, -13593, -959, 2061, 26361, -4728, 19975, -708, -12117, -4353, 25676, 10824, 20299, -25227, 27951, 24086, 1701, 30140, 12231, -31080, -32141, 9642, -5982, -19778, 17301, -882, -2171, 9471, -11549, -21644, -28491, 1911, -3420, -6993, 2698, -26785, -12938, 17205, 4662, 10951, 4420, -26717, 16447, -26879, 8764, 10883, 13861, 7424, -13674, 2895, 22221, 3930, -1521, 20057, -8017, 26469, -16194, 2164, 2436, -12133, -29954, 8735, 22365, 19743, -32106, -7955, 16923, -4264, -29129, -20375, 749, 699, -22889, 4605, -13245, -21195, 9930, 1306, 3319, -26951, 20953, -16852, 19030, -22993, -23164, 23975, -3038, 21137, 31580, -9436, 16986, -30515, 10741, 11808, 30744, -10067, 9787, 15804, 17637, -7855, 26538, 9597, 30972, -22636, 22846, -4288, 3577, -23402, 10439, -14678, -27151, 19243, 17932, 26409, -25288, -4566, -18636, -582, 17547, -21996, -24735, 11413, 27773, -337, -25077, -8806, 12140, -19134, 25320, -23296, 196, 17390, 2406, -12967, 21005, 28688, 21856, 5159, 25877, 19326, -31171, -26836, 28888, -27609, -11307, -13309, 6774, 7813, -6624, -24364, -10646, 23713, 4636, 16555, -29628, -5704, 8823, -15616, -31671, -11868, 28918, -5702, 31460, 15852, -31226, -21123, -25572, 9341, 11100, 15714, -22771, 15979, -295, 28946, -20460, 6924, -31371, 18348, 11338, -11866, -24089, 30587, -6604, -11808, 21968, 2274, -29355, -2835, -8059, -2466, -924, 8876, 1555, 12075, 9768, -8975, 29280, 23968, -17734, -12593, 28486, 15677, 10777, 16874, -8789, 530, 17539, 30824, -12683, 4332, -18032, -29786, 32273, -28393, -22468, 25712, -30445, -16343, 769, -27147, 6769, 25822, 17175, -29300, 12031, -23756, -19162, 27109, 23061, -5143, -21790, -955, -8201, -24023, 25498, 10755, 23950, -10185, 5960, 22816, -16524, -1580, 17756, -32697, -28548, 29164, 607, -22902, -2719, -8248, 25855, -22418, -15068, 11755, 22865, -21321, 1770, 320, 26455, 9885, 24977, -8778, 1609, -15130, -17648, 25306, -21976, 8161, -6320, 16205, -5950, -23638, -8982, -32225, -27095, 22976, 23711, 19139, -30973, -13241, 420, -588, -22983, -6891, 25570, 2683, -8469, 23907, -4754, -5261, -2734, -20058, -30358, 28729, -18374, 6411, -18669, 28006, 10151, -397, -22097, 10075, 9578, -4910, -12083, -8194, 32645, -16073, 26932, -28393, 14541, -20945, 32084, 2496, -22525, -2101, 30526, -14640, 32465, -15367, -18791, -17877, 12751, -4063, -13678, 32441, 9709, -21349, 31329, 20950, 9575, -11425, -10766, 11062, -2619, 17005, 27391, 15934, -20043, -14199, 12796, 1322, 24222, 10711, 5017, 11756, 4701, 17405, 30141, 9908, -7667, 23430, -283, -26535, 30646, 9434, -10006, -24557, 17033, 3418, 3944, -31851, -18522, 16050, -28812, 10942, 3794, -7475, 15725, -1892, -19498, -12016, 19019, -4247, 28594, 32531, 30438, -14290, 29693, 22512, 2509, 11596, -14912, 18402, -3576, 30905, 23106, -20015, -2089, 20779, -10548, 5745, 31355, -32181, -25566, 31189, -18482, -23344, -7770, 25132, 28636, -23073, -16092, 15911, 17079, 12995, -3298, 29623, -15419, 22656, -2238, 23951, 29883, 19533, -20073, 9565, 17120, 18563, -6230, 14181, -17190, 2588, -25336, -8880, -16198, -10148, 14060, 19767, -15887, -30758, 17337, -25351, -29499, 26685, 16754, 8751, 18214, -21274, -25683, 1476, -7395, -13689, -10195, -96, 194, -22480, 8026, -22200, -31310, -8494, 28738, -4504, -10461, -17629, -10619, -5934, 15426, -9517, 20069, 8079, -5660, -9896, 30407, 18673, -4822, -8581, 29233, 19180, -647, 18846, -6609, -7743, 19753, 15313, -10560, 23142, 15192, 31645, -28475, -12901, -19983, -652, 29069, -31757, -13162, -5053, -18225, -21091, -18929, -21519, 2033, 26612, -29355, 23880, 21570, -8792, -4720, -15104, 27111, -3679, 28163, -3680, 22345, 9589, 30467, -31553, -6516, 9025, -2010, 18020, 6294, -9040, -30314, 31675, -13071, -15877, -4849, 17922, 15492, 17358, -2826, 20585, -28254, 31194, 14946, -15585, 17993, -10694, 3537, 11895, 9330, -27208, 5582, 29262, -5835, -17483, 29133, -13662, -25912, 17987, 17908, -11418, 4011, -19921, 18677, 7752, 7584, 25936, 18110, -5054, -26013, 5158, 3757, -24472, -1601, 30495, 9654, -11089, 30547, -4561, 26524, 17189, 11153, 11076, 20283, 1723, 7036, -29486, 23767, 30180, 29853, 31149, 7626, 7371, 30175, -1631, 6588, 16169, -13654, -11937, 32048, 19121, 2900, 6973, -26282, 29194, 4609, 63, -14527, 4098, -4238, -11610, 29283, -28467, 31691, 26327, -20257, 31223, -25231, 22984, 24651, 24154, 22378, 2152, 7420, 22182, 31599, -29076, 31063, -29834, -27353, 19751, 29512, 20748, -21838, 21553, 17398, -9594, 30347, -10373, -27246, 388, 9373, 25489, 21971, -4972, -7761, 7529, 2663, 994, 31393, 26064, 5280, 31687, -4320, 1455, 21616, -25636, -4992, -32171, 28361, 17808, -4840, -782, 30963, 6014, 26744, 12210, 4633, -13128, -5907, -8118, -5737, -28849, 21164, 5432, -29079, -22484, -20192, 24489, 13540, 9443, -20719, 31644, -728, -7331, -24172, -22206, -143, -4766, 702, -8488, 30596, -26063, 3180, -22724, -9407, 18194, -6751, -19867, 29082, -22918, -17875, -2267, -28052, -10300, -863, 25344, -13351, -25523, -32710, -23802, -30021, 12822, -17486, -21980, -12096, -4797, 1542, -7526, 11794, -11217, 8822, -22466, -6535, -4467, 21905, -24659, 6028, 25357, -661, 19236, 27173, 22047, -10825, -18552, -13717, -17312, 15476, 7617, -11566, -21378, 16354, -16368, -28664, 21978, -17108, -26959, 29036, 21435, -7042, -30266, 5849, -1257, -19973, 7602, -25039, -29043, -29405, -20285, 2963, 7795, -15987, 16564, -5156, 16332, -8375, -30680, -26802, -32267, 28162, -25906, 8546, 23862, 18335, -6873, -22697, -21652, 31637, 980, 23193, -25016, -16421, -27909, 12574, -7064, -13444, -26570, 8893, -22472, -15899, -9396, -3151, -15232, 12345, 23031, 12771, -14983, 25272, 3543, 25826, -12208, 30499, -23424, 30296, 9608, 8012, -18405, 28902, 19953, -24629, -6777, 21972, -28972, -24369, 16369, 10997, -31555, 31826, 15155, -12169, -13410, -7584, -15448, 7899, -27847, 6140, -28146, 15216, 12994, -9320, 28271, -4764, 32411, 23761, -5124, 25757, -2908, 18681, -30557, 12109, 15297, 2045, 23324, -21253, 334, 8779, 31, 8938, -7255, -7195, -24553, -11006, -2548, 9704, 30737, -11532, 18389, 1037, 1091, 30700, 19126, -2162, 410, 6704, 4073, 13364, 22780, -21584, -10913, -14042, -23887, -7814, 2038, -27249, 690, 2380, -19719, 23111, -31312, 3274, 3878, -1342, -18113, -13512, 32726, -1439, 4776, -28633, -13296, -4866, -29804, 20024, -2051, -24097, 1622, -22262, -7019, 1158, 17905, -7012, 13314, 20828, 1332, -30498, -4668, 32110, 8523, 27510, 15732, 4924, 22551, 28739, -28294, 3346, -4104, 26161, -24014, 13230, -11269, -21992, 9458, -10635, -10835, -30039, 30623, 23838, -8546, 3724, 15597, -20253, 19547, -5201, -24263, 5559, -17004, -17153, 5426, -32533, -32566, -3221, -23182, -3663, 310, 24818, -19043, 2406, -6196, -4751, 22125, 22105, 10314, -23693, 9637, 7567, 3780, 23926, -3098, -26449, -26584, -19788, 3399, 31539, 24983, -16254, -20678, -4277, 31389, 32490, -5956, 6331, 30238, 26571, -13619, -6593, -17037, 17085, -9878, 19613, -4327, 16051, 19579, -2570, -6320, 7807, 30014, -22871, 24934, 6606, -4189, 21131, 22796, -12625, 1323, -1689, 23568, -8623, -25885, 4213, 21985, -23733, -4029, 25930, 15513, 32738, -19223, 12397, 26502, 9518, -32417, -3186, 21617, -11102, -23809, -24321, -19503, -16782, -17290, 29109, 25317, 14909, -29906, 24791, 22243, -19191, -30074, -30558, 29613, 16234, -16208, 1033, 17208, -21941, -29419, 6525, 5222, -4935, 6602, -2831, -23811, -22030, -27884, -16788, 3319, -18830, -23683, -18738, -12264, -12676, -28434, -26219, -23939, -21328, -17735, 6628, 2019, 21201, -28412, 5194, 32361, 23089, 26613, 15999, -21410, 16092, -3029, -7096, -25235, 616, -20085, -6418, 17335, -10247, 13369, -26523, -9467, 20597, -30316, -4977, -26616, -4108, 31663, 1916, 7263, 3285, 9592, -12807, 22946, 19982, 26317, -14023, 19107, -10602, -28595, -4412, 6899, 16285, 28224, -4879, 10778, -11725, -25209, -22681, -25148, -24084, 6451, 5183, -25214, -13620, -31890, -28241, -2762, 3688, 21076, -30169, 28683, 2651, 14778, 4492, 16080, -10873, 15047, -26956, -23430, 21378, -16493, 30691, 2049, -21457, -8490, 4512, 22238, -16630, 11367, -16488, 7225, 10073, -30805, 32039, -9758, -1800, -25995, -17684, 8606, -725, 20329, -14850, 18755, -17537, 14430, -26144, -30539, 17668, -32004, 5908, 15302, -24875, 12054, 16804, -32284, 9295, 10641, 19301, -1719, -10428, -23948, -15504, 347, -25867, 18962, -26484, -16666, 18728, -28752, 359, -22058, -29824, 23623, 841, -12727, 30077, -6086, 5627, 18918, -9323, 21021, 18673, -24235, -2161, 1520, -10956, 14316, 19452, 3521, 10494, -16128, 18363, -16488, -21933, 28509, 19658, 17968, -630, 61, 19967, -4115, 8022, -18416, -24662, -31330, -26649, 2616, 27961, -2322, -1467, -15827, 4811, -1315, 18455, -4300, -27395, 9469, 28204, -21356, 17317, -10077, 20675, -10062, 5849, 21554, -10375, -17740, -24623, 7939, 92, 8461, -13392, -32274, -21303, 19794, 22343, -28870, -12765, -18358, -3061, 22707, -16354, 1323, -5679, -29888, -21823, 10467, -5144, 5772, 7737, -22459, 10591, 21687, -3738, 30489, 2364, -9793, 2416, 14585, -26381, 7843, -16800, 27357, 13073, -30170, -8097, -8181, 5822, 32546, -16903, -3672, 9915, 18961, 29606, 20316, 26987, -20029, 16640, -25340, 9026, -6687, 13697, 15011, 542, 27351, -14, 815, 23463, -831, -26347, -20695, -6654, 11199, -3000, 7854, -9040, -22958, -7382, -7134, 16838, 24463, -14086, -16213, 9940, -23474, 971, -13013, -13001, -6055, -29612, 2930, 923, -9596, -15150, 4583, -27640, -28787, 25784, 15831, -7232, -19618, 4494, 6155, 16938, -629, -13928, -13020, 5933, -31970, -743, -28906, 29138, 1587, 4607, -29123, -27851, -1671, -22074, -31540, 7490, -15942, -31713, -16632, 14845, -21280, 9432, -11564, 30551, 10040, 32512, 6106, 21243, 16154, 12264, -16268, 1419, 19406, -21068, 30720, 916, 13531, -1656, 4297, -6034, -2492, -18133, 26406, 16309, 2587, 9671, -23609, 6092, 21470, 20956, 19470, -5743, 29509, 31931, 19995, 2828, 3438, 11464, 21546, 24672, -7807, 18201, 211, 10202, 26626, 27156, 31560, -14176, 26039, -14473, -12107, -13504, -16901, -27334, -26040, 19906, -24049, -5947, 3690, -29315, -18278, 25079, -9677, -24087, -7660, -1972, 15405, 3128, -26048, 17500, 298, -3966, 32120, -17730, -3588, -3763, -19738, -6723, -32748, 293, 5500, -1477, 29161, 3008, 30769, -24937, 10972, 9268, 22303, 25756, -20735, -14001, -15032, -4108, 23927, 29978, 24963, 9549, -31546, -18930, 28967, 30535, -10955, 3872, 16217, 28554, 10292, -10404, 14990, -32203, -27545, -27112, -9598, -21761, -14845, -28806, -12609, 32518, 12085, 24859, 9768, 15293, -5516, -11166, 8103, -31966, -14960, -6840, -22207, -31725, 31442, -8918, -23025, -3241, 19149, 16854, -32010, -14952, -29995, -1234, 4788, 14001, 27772, -31682, 26516, 2247, -12039, -2083, -14757, 26799, 17757, -9603, 22780, -2211, 19430, 5771, 10581, 13506, -26662, 5330, -14677, 22937, -18274, 22321, -29534, -21270, 15179, 18636, -24838, -28745, 263, 14263, 23244, 30251, -10470, -17978, -18078, 10373, 3006, -1519, 21603, 17636, -20198, -7052, -10525, -13869, 1382, 15881, 3354, 1170, 28290, 12473, -18724, 9902, 16902, -6676, 28841, -2035, -30433, 19938, 13656, -17585, -23875, -17066, -30718, 23384, 27562, -16538, -28078, 19729, 32369, 29359, 23536, 13787, 10735, 832, -22270, -19199, 21026, -30416, 8686, -23888, 7218, -9335, -15510, -8500, -4335, 2010, 20606, 29000, -25430, 32117, 5892, 7695, -18243, -5124, -9852, -17538, -10187, -16519, -10240, 18919, 20370, -23538, -20203, -7861, -6913, -19980, -25092, -23280, -22365, 23660, 12323, 27800, 18542, -9172, -24797, -7844, 31322, 17136, 11363, -22319, -10024, -12969, 9715, 18479, -3373, -7296, 15429, 22389, 30870, 15096, -9269, -20998, -8504, 8500, -29408, 12976, -9155, -856, 13512, 8456, -7133, -7308, -7440, -19854, -6806, -6296, 13792, 30170, 24353, -2646, -26081, 10903, -31633, -8514, -18595, -19287, -19008, 17595, -1051, -3700, 14526, 5140, 10528, 31304, 9613, -20884, -22624, 14817, 11216, 27723, 11558, 27358, 16482, -20123, -8412, -25678, -30069, -520, -5107, -29928, 31795, -16357, -26299, 30436, -18487, 3459, 18184, 21959, 20069, 15072, -29883, -29820, -25458, -21109, -19786, 28897, 19833, -31896, -24418, 14009, -28952, 1495, 14959, -2132, 27539, -30552, -26513, 6270, -4695, 27286, -26151, 5547, -13407, 5008, -11021, 3063, 20879, -28127, -24402, -7434, -8332, 5728, -5988, 15036, 31327, -5124, -11090, 5546, -24778, 3147, -14863, 28571, -23254, -29734, 12949, -22246, 28366, 17448, 21820, -18414, -10206, 17197, 21520, -20887, 19693, -3236, -23166, -19908, -9869, 6044, 15503, -25451, 13521, 11657, 10650, 13580, 7139, 25943, 21350, -20387, -18166, 6541, -12226, 1657, -4987, -7748, 31523, -17128, 29982, 5992, -21137, 29552, -21623, 10604, -27825, -13073, 22311, 5885, 21565, 1105, -30425, -18231, 27930, 8008, 3956, -23221, -17755, 24630, -6002, -7044, -30325, 31220, 1944, 5708, -9803, 19151, -7238, 30020, -8689, -25785, -8438, -6251, -18015, 22656, 24985, -2212, 23583, 12196, 6131, -29973, -31941, 6755, 22287, -16486, -5304, 16086, 32484, -29850, -16863, 8840, 12913, -8375, -5981, 24619, 9137, -12316, 27513, 18246, -9274, 19958, -19613, -7980, -19990, -19023, -19163, -2753, 14592, 111, -21706, -13787, 12188, 7976, -23461, -10759, -30974, 7301, 32652, -30229, 996, 27050, 26180, -13653, -24089, 10846, 5247, -18699, 32409, -29064, 3972, -4381, -4701, 3090, -6017, -7834, 874, 19324, -21596, -1314, -26629, -28050, 1626, 24831, 11357, 5447, 25217, 19852, 17399, 20995, -21173, -7802, 13284, 26229, -17408, -18601, 25267, 31053, 28130, 3795, 17378, -27116, 2234, 3775, -27967, -8416, 3819, -21208, -32136, -15024, 22750, 30260, 1521, 27278, 18613, -3150, -14420, -12714, 714, -4326, 24006, 12414, -2734, 22372, 16868, 23685, -14206, -15356, 19350, 28739, -8861, -13585, -19642, 18782, 23532, 13832, -27681, -24005, 9792, -28319, 19526, 5650, 15998, -20430, -5521, 12723, -15161, 31746, 12677, 23028, 19030, -21746, -27590, 10517, 27332, 7897, 31348, -13081, -21196, -19214, -22812, -19717, -14773, -3894, -26969, 31330, -14829, -3870, -24239, -13724, -4238, 6015, -18655, -22044, 10178, 13006, 574, -21386, 1745, -21672, 23502, -19196, 14388, 30522, -21305, 18269, 1328, 26720, -15966, -16635, 17750, -9479, -26078, 28447, -31880, -12473, -2032, -21006, -10872, -13561, -27307, 8203, 16331, 27136, -8048, 30409, 3369, 1784, -9508, -603, -27352, 22673, 20472, -6037, 29902, -2398, -13795, 8109, -15348, -29860, 31383, 18651, 29947, -9670, -12600, -18000, 15174, -469, 11266, 24803, -4767, 205, 20732, 16369, -3696, -31530, 5177, -20474, -29691, 25813, -4316, 8778, -26778, -14969, 24578, 23971, -28429, -16020, -26322, 29575, 25676, 7728, 7152, 13150, 10551, 4421, 16329, 26404, 31563, -16422, 15168, -5330, -691, -12354, -10417, 19286, -29127, 1153, 7684, 14044, 10549, -32745, 22190, -5289, 27873, -228, 31582, 28157, -9889, 18560, 12769, -8887, 4282, 20908, -494, 19109, -17922, 17734, -20442, 18030, 21324, -13685, 21985, 10778, -3146, -16221, 17548, -32520, 16619, 3167, -22671, 14075, 29039, -633, -16855, -5673, -30330, 14522, 19809, 32661, 26063, -11287, -27015, -16499, 18140, -8750, -28430, 6190, -29981, -5285, -18399, -2862, -12328, -6648, -16092, -5362, 11879, 8004, -14012, -29360, 28673, -16529, -7109, -16392, 22181, -31921, -19909, -31192, 25670, -886, -25430, 29599, -22671, 24848, 7005, -19758, 4836, 7225, -8222, -32555, 9698, -17023, 22013, -6858, 22962, 2704, -16042, 4444, 11232, -18467, 26907, 26381, -26913, -23311, -24421, 1701, 1286, 20141, 27876, 4819, -87, 24590, 1944, -7216, -16169, 15105, 26502, -18601, -14918, 25033, -31520, 24567, -30616, 17503, 15304, -17088, -2479, -29197, 8446, -15747, 8129, 20775, 20707, -11230, -5032, 10930, -26832, 20016, 41, -1477, -29726, -13618, 15074, 28900, 29800, -26732, 25367, 3238, 30144, -29747, -23886, 1195, 29438, 21958, 24793, -406, 10806, -23521, -11801, -32673, 26588, -9037, 32627, -2688, 25135, 23470, -303, 12413, -3982, 10033, -7398, -16645, -32453, 2851, 22232, 28941, -5547, -12284, -24906, 12783, -8228, 22367, -1863, 10145, -19609, 7602, -27101, 31350, -5078, -22608, -17389, 13408, -11089, 29170, 16136, 13011, -19003, 19206, 27712, 28872, -22698, 25920, 22928, 25354, 27262, -29843, -31939, 13759, 15052, 12057, 21172, -2999, -25291, 11961, 24011, -30519, -9919, -19869, -10833, -21547, 32302, -32669, 1135, -6990, 7304, -11406, -4562, 23102, -7192, -24767, -19641, 21806, 29086, -21070, 26028, 4936, -21949, -22690, 3664, 7645, -23736, -32695, 19768, 15728, -4672, 20870, -14686, 12651, -8320, 5241, -14339, -2016, -29160, 18705, 20708, 15369, 31211, -21049, 12151, -15134, 24076, -17798, 25947, 7974, 15562, 31672, 10942, -7436, 467, -4267, -6390, 32680, 31957, -4320, 15625, -28334, -8150, 1804, -19567, 286, -6252, 18546, 23496, -9539, -3316, 5016, 5370, -18273, 4571, 27950, -25771, 25762, -27494, -8800, 672, -6822, 19522, 13677, 4664, -3549, -14730, 25579, -2774, -26883, -21779, 13305, 3526, 9367, 29538, -27564, -16325, 29416, -23707, -15312, -14563, -15796, -840, 5218, -22745, -2950, -19098, -5508, -32254, -18885, -20038, 14529, -30084, 14803, 849, 24860, -20, -12045, -27373, 4634, 2075, 30639, 11734, 29620, -15234, 23095, 14285, 19948, -23550, 8630, -5399, 28282, 26485, -21886, -13824, 21497, 3181, -1898, 9293, 11692, 10536, 9142, 11433, 4311, -4662, -16975, 9871, -3125, 395, -5030, -14821, -751, -28656, -26702, 5668, 5116, 13458, -10219, -23751, -10612, -18568, 26878, -24226, 15618, 10820, 17215, -3275, 1174, 9738, -1013, -25299, -7376, 339, 24418, 24237, -22578, -29126, 14022, 19762, -25164, 27760, -19384, 16754, -11426, 32283, 10442, 25041, -7124, -26376, 17369, -23195, -23590, -32363, -28386, 32334, -14555, -25961, -12403, 10946, 28186, -31285, 18231, -53, 13077, -4721, -24230, 21824, 3666, 26373, -5836, 18422, 28244, -6277, -30391, -9015, -30119, -26226, -6922, -29029, -20600, -29030, 16444, 32375, 14735, -18473, 17792, 27450, 16106, -3961, 983, 2283, -27137, 9443, -26573, -15089, 31595, 17610, 8082, -26677, -6888, 26384, 21845, -14016, -22547, 11785, -6373, -9021, 24476, 376, 21757, 7117, 15616, 22639, -16323, -30114, 5984, 24386, -10261, 32730, -21205, -13639, -5115, 29240, 29272, -11815, -7331, 25976, 14550, -32752, 1456, -29649, 19498, 3298};

  • If you didn't add "white_noise.h" header file then you should get Undefined IR build error" if you didn't get an error then you should have the IR declaration in "DSK6713_AIC23.h" or "header.h" header files.

    What do you mean by working and not working ?
  • Hi Titusrathinaraj Stalin,

    Maybe this helps to understand it better...
    Big Thank you !

    Im working with CCS5v5 on Win7, DSK6713.

    I have tow different c Files and one header(white_noise.h).

    There are two different scenarios

    I can build and debug, and it works-> with adding the header white_noise.h and with N=128(in NLMS.c, Filter coefficients)
    I can build and debug, and it doesnt do what it should do by -> adding the header white_noise.h and with N=256 (in NLMS.c, Filter coefficients)
    Idk Why ? I dont use the header(white_noise.h). I guess there is a time problem with the interrupt?

    Thank you so much for reading! regards Daniel


    white_noise.h
    short IR[8000]={23670, -2424, -25025, 23474, 32467, -10922, -5724,....


    -----------------------------------

    NLMS.c
    //Optimization Level 2

    #include "refnoise.h" //cosine 312 Hz
    #include "dplusn.h" //sin(1500) + sin(312)


    //#define mue 1E-10 //rate of convergence
    #define N 128 //# of weights (coefficients)
    #define NS 128 //# of output sample points
    #define delta 1E-10
    #define alpha 1E-3
    float w[N]; //buffer weights of adapt filter
    float delay[N]; //input buffer to adapt filter,x
    short output; //overall output
    float yn, E; //output filter/"error" signal

    float gamma=0.01;
    float Px=4500.0;
    float mue = 1E-10; //rate of convergence
    float mue2;
    short input_option=1;

    short NLMS_function()
    {
    static short buffercount=0; //init count of # out samples

    delay[0] = refnoise[buffercount]; //cos(312Hz) input to adapt FIR

    Px= (1.0-gamma)*Px + gamma*delay[0]*delay[0];

    short i;
    yn = 0; //init output of adapt filter
    for (i = 0; i < N; i++) //to calculate out of adapt FIR
    {
    yn += (w[i] * delay[i]); //output of adaptive filter
    //Px= (1-gamma)*Px + gamma*delay[i]*delay[i];
    }

    E = dplusn[buffercount] - yn; //"error" signal=(d+n)-yn

    mue= 0.01/(Px*N+delta);
    for (i = N-1; i >= 0; i--) //to update weights and delays
    {
    w[i] = w[i] + mue*E*delay[i]; //update weights
    delay[i] = delay[i-1]; //update delay samples
    }


    buffercount++; //increment buffer count
    if (buffercount >= NS) //if buffercount=# out samples
    buffercount = 0; //reinit count


    output = ((short)E*10); //"error" signal overall output


    return output; //return from ISR
    }

    ------------------------------------------------------------------------------------------------

    main.c

    #include "DSK6713_AIC23.h"
    //#include "white_noise.h"
    short NLMS_function();
    Uint32 fs= DSK6713_AIC23_FREQ_8KHZ;

    //Define
    #define LEFT 0 //stereo
    #define RIGHT 1 //stereo

    short input;

    interrupt void c_int11() //ISR
    {
    DSK6713_LED_on(0);


    output=NLMS_function();
    output_sample(output); //overall output result


    DSK6713_LED_off(0);
    return; //return from ISR
    }

    main()
    {
    DSK6713_LED_init(); //init LEDs

    short T=0;
    for (T = 0; T < 30; T++)
    {
    w[T] = 0; //init buffer for weights
    delay[T] = 0; //init buffer for delay samples
    }
    comm_intr(); //init DSK, codec, McBSP
    while(1); //infinite loop //infinite loop
    }
  • Daniel,

    You have said that with only changing the comment on the white_noise.h include line, it affects the results. But as we said earlier that should not make a difference if you are not using it. Now you are saying the difference is N=128 or N=256:

    Daniel Zapa said:
    I can build and debug, and it works-> with adding the header white_noise.h and with N=128(in NLMS.c, Filter coefficients)

    I can build and debug, and it doesnt do what it should do by -> adding the header white_noise.h and with N=256 (in NLMS.c, Filter coefficients)

    Idk Why ? I dont use the header(white_noise.h). I guess there is a time problem with the interrupt?

    In both cases you are adding the header white_noise.h, and you are using different value of N. Your guess of "a time problem with the interrupt" certainly sounds like a reasonable place to look. Please measure the amount of time it takes to execute the ISR by observing the LED that you are toggling. Measure it for the working case with N=128 and for the failing case with N=256. Also, not the time between LED_on to the next LED_on in both cases.

    What do you observe from those measurements? How do they compare with your expected operation of the ISR?

    Regards,
    RandyP

  • Hi Daniel,

    Daniel said:
    If am adding the white_noise.h, my program doenst work anymore! I dont use it.. just adding to my program. 
    If Im comment this line with my header... my program stil works.

    From the C programming perspective, when we write  -->  #include "filename.h" or #include <filename.h> in a *.c source file , it means it copies the complete content of the header file into the *.c file during the preprocessing stage.

    In your "white_noise.h" the IR array of data type short is defined. when you include this header file into your main.c, the content of white_noise.h will get copied before your main.c is processed. In your main.c, in the function, "interrupt void c_int11()" you are using the array, "IR".

    As a user of this code, you should go through the code in the header files and understand which values of the global variables will be used inside your functions and where it is declared and defined.

    when you say, if you don't include the header file, "white_noise.h", check whether the variables/functions declared/defined in that header file is used elsewhere in any of your source files. If the answer is "NO", then it is not needed to be included in the source file at all.

    or if you have commented the portions in your *.c file, which uses those variables in the header, then it would get compiled without any errors. But it does not mean that the program is complete.

    On your second post, I would like to recommend you to understand what is "N", what is the lower limit and what is the upper limit of "N". what is the significance in the algorithm if the N value is changed...Finding answers for these questions may give you some good understanding of your problem.