Hello,
Just wondering what this error means. Below shows the output window... FYI, I do not have an issue with another board assembly, just trying to decrypt the problem.
¯ -stdout
¯ -omap 3
¯ -t 60
¯ -p EVM_MDDR_MICRON_2G
¯ -2
¯ chip_erase NANDINFO 0
¯ Leaving parameter file:temp_script.txt
¯ @temp_script.txt
¯ Looking for device (omap usb)
¯ Please turn on device
¯ Waiting for device (omap usb)
¯ Found device (omap usb)
¯ Awaiting ASIC id
¯ AsicId items 05
¯ AsicId id 01 05 01 36 30 07 07
¯ AsicId secure_mode 13 02 01 00
¯ AsicId public_id 12 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
¯ AsicId root_key_hash 14 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
¯ AsicId checksum 15 09 01 13 BF 3E EF 00 00 00 00
¯ Searching 2nd for: EVM_MDDR_MICRON_2G 363007 07 GP
¯ Loading second file Targets\2nd-Downloaders\dnld_startup_omap3_gp_2g.2nd
¯ Entering parameter file:omapflash2nd.txt at line: 16
¯ -pheriphalboot_reopen
¯ Reading board configuration file Targets\Configurations\configuration_evm37xx_micron_2g.txt
¯ Reading definition file .\targets\definitions\definitions_omap3.txt
¯ -board_config Targets\Configurations\configuration_evm37xx_micron_2g.txt
¯ Leaving parameter file:omapflash2nd.txt
¯ Sending size of second file (0x00006804 bytes)
¯ Transferring second file to target (0x6804 bytes)
¯ Closing boot connection
¯ Found device (omap usb)
¯ Waiting for 2nd
¯ Found 2nd
¯ Looking for a driver for 'NANDINFO'
¯ chip_driver NANDINFO Targets\Flash-Drivers\nand_onfi_16bit_8bit.bin gpmc 0x6E000000 cs 0 address 0x28000000 bberase 0 onfi 0 bpp 2048 sbpp 64 ppb 64 bpl 4096 l 1 acv 0x23 f 0x0019
¯ Downloading driver
¯ Operation FAILED (Remote: : Unknown command dri6er)
¯ Elapsed time: 0:00.000
Console program failed, exit code: 3
Any help would be appreciated...
Thanks