Other Parts Discussed in Thread: OMAP3530
Hi,
One of the customer is facing an issue while rebooting the device. Below are the descriptions.
Processor you are using : OMAP3530,
BSP version : 6.6.0
Platform (EVM or custom board) : Custom board,
Steps to reproduce the problem. : reboot the device using "KernelIoControl(IOCTL_HAL_REBOOT,NULL,0,NULL,0,NULL);"
then some time reboot and some times not, get stucked after XLDR is up with message "Jumpingto bootloader" this is a XLDRmessage before XLDRMSGDEINIT;
Thanks
regards
Sathish.