Other Parts Discussed in Thread: SYSBIOS
Champs,
I see in the SDK that for the IPU SYSBIOS is configured to run in SMP mode, so utilizing both M4 cores with single RTOS instance. The questions I have:
1. Is it possible to run 2 separate SYSBIOS instances for each M4 core on the IPU?
2. If yes - is it supported in the toolchain?
3. again if yes - what would it take to build and run separate applications for two M4 cores? Is there an example available?
thanks
Michael