Hello, This is happening on the OMAPL138 SOM from LogicPD. Part number = OMAP-L138 SOM-M1 When passing the parameters for the CMEM, it does not follow the parameters set for the heap. The remaining parameters are followed. It always places the heap buffer at 0xC300 0000. But we want it at 0xC700 0000, which is in the parameters we set for the CMEM.
Is this hard coded? What is the work around for this?
Thanks.