Other Parts Discussed in Thread: OMAP3530
My customer has a couple of questions about using the CSI1b interface on the OMAP3530. He has a CUS package, so he cannot use CSI2, for which we actually have a driver available (WInMo, but it's close enough to WInCE for him to be able to use), so he will have to make some changes. The following HW questions I have not been able to answer, please help:
1. When only using CSI1 (cam_d6 through cam_d9) can the other camera bus bit be left floating or should they be pulled ?
2. For the MIPI use on the receiving end at the OMAP is there any need for external termination resistors like 100 ohms for subLVDS? Is that built in the OMAP?
Any help on this would be appreciated.
Regards
Tiemen