Other Parts Discussed in Thread: AM3357, TPS65910
We have set UART0 to boot in our AM3357 Application board with sysboot configuration [15:0] = 01000000000010 (UART0, SPI0, NAND, NANDI2C).
We have used the same PMIC which is used in EVM (TPS65910), all supplies are stable power ON reset is de-asserted.
When i power-up my board, It should send out a "CC...." on terminal, but nothing is comming out. the UART0_TXD line is always High.
When we checked clkout1 by setting sysboot[5] to high it was 24MHz same as I/P to the processor.
We also checked VDDS_PLL_MPU, VDDS_PLL_DDR & VDDS_PLL_CORE_LCD power supply which is 1.85V.
What else should we do to get "CC...." on UART0. Any help or suggestion to solve this is appreciated.
Vasanth T P