Hi,
The ISDK v01.00.00.07's Known Issues in the release note doesn't mention about the
issue "Inconsistency of 64-bit DC System Time".Can we assume this issue exist in v01.00.00.07 also?
If that is true, is there is way to overcome this issue and continue to use v01.00.00.07?
the latest version v02.01.02.02 seems have fixed this issue but we need to continue using
v01.00.00.07, it will be very helpful if there is any software patch to FIX the issue in v01.00.00.07.
Best Regards
Kummi