This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[OMAP L138] Compiling a kernel for HawkBoard using L138 SDK

Hi !

I have the OMAP L138 SDK downloaded from here: http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/omap_l138/1_00/latest/index_FDS.html

I am trying to compile a kernel for Hawkboard using the source code given in the OMAP L138 download page, but it is giving some errors. I also saw that it is not having an option to configure a kerne for Hawkboard in the "system type" when I do "menuconfig".

Is there a way to compile a kernel for hawkboard using TI's OMAP L138 sdk? If yes, can you please upload the .config file for it?

Thank you.