i create a new project with main.c for a15 baremetal and add a asm file in which i have a function defined that i want to use in the main.c
when i build the project i get a warning
arm-none-eabi-gcc: warning: ../myasm.asm: linker input file unused because linking not done
Finished building: ../myasm.asm
followed by
makefile:143: recipe for target 'asmtest_CSL.out' failed
Are there any extra build options that i am missing?
i am using the following:
CCS 6.1.3
GNU 4.9.3(Linaro)