we have 3rd party WLAN component from Broadcom, They provide the driver as KO file. we using Linux kernel 3.8 as a base and jacinto 6 is the platform.
the WLAN SDIO lines are connected to MMC1. There is a GPIO wake line connected to the SOC pin. what are the necessary kernel changes required to enable this component. how to indicate the middleware layers about the SOC connection with the WLAN components and the GPIO pin.