This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

can not access C5515 GPIO12 to GPIO20

Hi,

I am using C5515, I want to use GPIO12-17 and GPIO18-19 as well. Currently EBSR = 0x1800 meaning it it's configured to use SPI(7), UART(4), GPIO(6) and IIS(4) pins.

I do not need IIS pins instead I want GPIO access on those pins.

I could not find any configuration in EBSR nor any supporting documents that can allow me to use UART,SPI and GPIO12-20.

Is it even possible to use GPIO12-20 while still keeping SPI  and UART mode intact?