This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5150 streaming issue

Other Parts Discussed in Thread: TVP5150, TVP5150AM1

Hi,


We are using ti-ezsdk_dm816x-evm_5_05_02_00 and Linux 2.6.37 software and

We are using our customized DM8168 board with TVP5150 decoder chip for video capture.

When we run saLoopBack application, the video is successfully streamed from the TVP5150 decoder chip, but we are seeing some interlaced lines on the display during the motion, not observed in the static area.


Please help us to know what could be the reason for the lines and how could we resolve it.

Regards,

Geetha

  • Current TVP5150 Register Settings

    tvp5150: Video input source selection #1 = 0x00
    tvp5150: Analog channel controls = 0x15
    tvp5150: Operation mode controls = 0x00
    tvp5150: Miscellaneous controls = 0x6f
    tvp5150: Autoswitch mask= 0x00
    tvp5150: Color killer threshold control = 0x10
    tvp5150: Luminance processing controls #1 #2 and #3 = 60 00 00
    tvp5150: Brightness control = 0x80
    tvp5150: Color saturation control = 0x80
    tvp5150: Hue control = 0x00
    tvp5150: Contrast control = 0x80
    tvp5150: Outputs and data rates select = 0x47
    tvp5150: Configuration shared pins = 0x08
    tvp5150: Active video cropping start = 0x0000
    tvp5150: Active video cropping stop = 0x0000
    tvp5150: Genlock/RTC = 0x01
    tvp5150: Horizontal sync start = 0x80
    tvp5150: Vertical blanking start = 0x00
    tvp5150: Vertical blanking stop = 0x00
    tvp5150: Chrominance processing control #1 and #2 = 0c 54
    tvp5150: Interrupt reset register B = 0x00
    tvp5150: Interrupt enable register B = 0x00
    tvp5150: Interrupt configuration register B = 0x00
    tvp5150: Video standard = 0x00
    tvp5150: Chroma gain factor: Cb=0x9a Cr=0x6c
    tvp5150: Macrovision on counter = 0x0f
    tvp5150: Macrovision off counter = 0x01
    tvp5150: ITU-R BT.656.4 timing(TVP5150AM1 only)
    tvp5150: Device ID = 5150
    tvp5150: ROM version = (hex) 04.00
    tvp5150: Vertical line count = 0x020d
    tvp5150: Interrupt status register B = 0x87
    tvp5150: Interrupt active register B = 0x00
    tvp5150: Status regs #1 to #5 = 1e 08 24 7d 81
    tvp5150: Teletext filter 1 reg 0xb1 = 00 00 00 00 00
    tvp5150: Teletext filter 2 reg 0xb6 = 00 00 00 00 00
    tvp5150: Teletext filter enable = 0x00
    tvp5150: Interrupt status register A = 0xc0
    tvp5150: Interrupt enable register A = 0x00
    tvp5150: Interrupt configuration = 0x04
    tvp5150: VDP status register = 0x40
    tvp5150: FIFO word count = 0x00
    tvp5150: FIFO interrupt threshold = 0x80
    tvp5150: FIFO reset = 0x00
    tvp5150: Line number interrupt = 0x00
    tvp5150: Pixel alignment register = 0x004e
    tvp5150: FIFO output control = 0x01
    tvp5150: Full field enable = 0x00
    tvp5150: Full field mode register = 0x7f
    tvp5150: CC data reg 0x90 = 00 00 00 00
    tvp5150: WSS data reg 0x94 = 00 00 00 00 00 00
    tvp5150: VPS data reg 0x9a = 00 00 00 00 00 00 00 00
    tvp5150: VPS data reg 0xa2 = 00 00 00 00 00
    tvp5150: VITC data reg 0xa7 = 00 00 00 00 00 00 00 00 00
    tvp5150: Line mode reg 0xd0 = ff ff ff ff ff ff ff ff
    tvp5150: Line mode reg 0xd8 = ff ff ff ff ff ff ff ff
    tvp5150: Line mode reg 0xe0 = ff ff ff ff ff ff ff ff
    tvp5150: Line mode reg 0xe8 = ff ff ff ff ff ff ff ff
    tvp5150: Line mode reg 0xf0 = ff ff ff ff ff ff ff ff
    tvp5150: Line mode reg 0xf8 = ff ff ff ff