Other Parts Discussed in Thread: DA8XX, TLC59108
I tried to probe da8xx-fb driver. ( Linux version is 4.4.12 )
I've changed defconfig file as below.
/arm/configs/am335x-evm_defconfig
# CONFIG_FB_IBM_GXT4500 is not set
-# CONFIG_FB_DA8XX is not set
+CONFIG_FB_DA8XX=y
# CONFIG_FB_VIRTUAL is not set
# CONFIG_FB_METRONOME is not set
# CONFIG_FB_MB862XX is not set
# CONFIG_FB_BROADSHEET is not set
# CONFIG_FB_AUO_K190X is not set
-CONFIG_FB_SIMPLE=y
+# CONFIG_FB_SIMPLE is not set
After compiling kernel driver source files, da8xx-fb.o was found in /drivers/video/fbdev/.
While running system, I can't find any log messages related with da8xx-fb. ( LCD not work )
[ 1.109012] of_graph_get_next_endpoint(): no port node found in /ocp/lcdc@4830e000
[ 1.117257] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.123993] [drm] No driver support for vblank timestamp query.
[ 1.146032] Console: switching to colour frame buffer device 100x30
[ 1.160635] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.191715] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.207478] loop: module loaded
[ 1.214299] libphy: Fixed MDIO Bus: probed
[ 1.281726] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.287901] davinci_mdio 4a101000.mdio: no live phy, scanning all
[ 1.294372] davinci_mdio: probe of 4a101000.mdio failed with error -5
[ 1.315664] cpsw 4a100000.ethernet: Detected MACID = 68:c9:0b:af:6e:14
fb_probe() is not called in da8xx-fb.c
Please let me know how to probe da8xx-fb.c