Other Parts Discussed in Thread: SYSCONFIG
I am using DM8168 custom board and the McBSP is not connected to anything, even I have configured McBSP Pin Mux properly.
I found I am not able to configure the McBSP registers, e.g., set RCR2 (0x47000118) to 0x1,RCR2 is still a "0" value not changing.
When I set SPCR2 0x470000110) to 0xc0, it still a "0" value. the value which read from XBUFFSTAT(0x470000B4) is 0x80.
Is there any extra steps to enable McBSP, in addition to McBSP clock setup from PRCM?
And, I did not find this DM8168 McBSP support from Linux PSP of dvr_rdk_04.
can any help me?