Other Parts Discussed in Thread: OMAP3530
Hi,
Starting from TI DSPLink examples (readwrite), I would like to send an image to the dsp-side for compression and then send it back to gpp-side. I first tried without doing any operation on dsp-side, just a loop. I have 2 problems.
1. With a .txt file it's working fine but with image (a small one) , I get an unreadable file !
2. I also changed memory map to use larger files but with a 1Mb image I don't receive any file back from the dsp-side, I get these errors
============= Sample Application : READWRITE ==========
Entered RDWR_Create ()
Leaving RDWR_Create ()
Entered RDWR_Execute ()
Buffer size: 1080054
file size OK
Size of file = 1080054
Unable to handle kernel paging request at virtual address c4b00000
pgd = c2f18000
[c4b00000] *pgd=82fb4011, *pte=00000000, *ppte=00000000
Internal error: Oops: 807 [#1] PREEMPT
Modules linked in: dsplinkk cmemk ipv6 minix
CPU: 0 Not tainted (2.6.32-rc2-davinci1 #1)
PC is at memcpy+0x50/0x330
LR is at 0xdbd6d6d6
pc : [<c0166870>] lr : [<dbd6d6d6>] psr: 20000013
sp : c3161da4 ip : d6d6d6de fp : c3161dcc
r10: bf11b168 r9 : 40b09008 r8 : deded5d5
r7 : d5d5d5d5 r6 : dadadad6 r5 : d6d6d8d8 r4 : d8e4e4e4
r3 : e1e1e1d9 r2 : 00057a56 r1 : 40bb9028 r0 : c4b00000
Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 0005317f Table: 82f18000 DAC: 00000015
Process waaves_decgpp (pid: 1639, stack limit = 0xc3160270)
Stack: (0xc3161da4 to 0xc3162000)
1da0: 84050000 00000000 00000001 00107af6 c4a50000 40b09008 bf101f14
1dc0: c3161df4 c3161dd0 bf0eed40 bf101f14 00107af6 00000000 84050000 00000001
1de0: 40b09008 00000001 c3161e24 c3161df8 bf0ee260 bf0eec2c 00107af6 40b09008
1e00: 00107af6 00107af6 00000000 bf11b178 00000000 84050000 c3161e5c c3161e28
1e20: bf0f000c bf0ee1e8 40b09008 c3161e38 00000000 00107af6 40b09008 00000000
1e40: 84050000 be9d5b9c c3160000 40025000 c3161e84 c3161e60 bf107248 bf0eff38
1e60: 40b09008 c3161eb4 00006c0c c3161eb4 00008000 be9d5b9c c3161eec c3161e88
1e80: bf109670 bf1071e8 c00888b0 c0074b64 c0029c00 00000000 00000200 c31a9ac0
1ea0: 00000000 0000006a 400b0000 c0494ec0 40023000 00008000 00000000 84050000
1ec0: 00107af6 40b09008 00107af6 c3161ed8 c2f4fa00 be9d5b9c 00006c0c c2f4fa00
1ee0: c3161f0c c3161ef0 c00aafa4 bf1091c4 c310e8a8 c2f4fa00 00000003 c2f4fa00
1f00: c3161f7c c3161f10 c00ab630 c00aaf3c c3161f34 c3161f20 c016ca88 c003acf4
1f20: 00000200 c208a700 c3161f44 c3161f38 c005cd94 c016c9e0 c3161f7c c3161f48
1f40: c0032780 c005cd94 c016c9a8 c003acf4 c3161f7c 00000003 be9d5b9c 00006c0c
1f60: c2f4fa00 c002d044 c3160000 40025000 c3161fa4 c3161f80 c00ab6cc c00ab0c8
1f80: ffffffff 00000001 00008eac 00000000 00008e00 00000036 00000000 c3161fa8
1fa0: c002cec0 c00ab69c 00008eac 00000000 00000003 00006c0c be9d5b9c 00000003
1fc0: 00008eac 00000000 00008e00 00000036 00000000 00000000 40025000 be9d5b84
1fe0: 00000000 be9d5ab8 0000bb68 40101aec 20000010 00000003 00000000 00000000
Backtrace:
[<bf101f04>] (MEM_Copy+0x0/0x18 [dsplinkk]) from [<bf0eed40>] (DM6467GEM_write+0x124/0x1cc [dsplinkk])
[<bf0eec1c>] (DM6467GEM_write+0x0/0x1cc [dsplinkk]) from [<bf0ee260>] (DSP_write+0x88/0xa8 [dsplinkk])
[<bf0ee1d8>] (DSP_write+0x0/0xa8 [dsplinkk]) from [<bf0f000c>] (LDRV_PROC_write+0xe4/0x180 [dsplinkk])
r8:84050000 r7:00000000 r6:bf11b178 r5:00000000 r4:00107af6
[<bf0eff28>] (LDRV_PROC_write+0x0/0x180 [dsplinkk]) from [<bf107248>] (PMGR_PROC_write+0x70/0xb4 [dsplinkk])
[<bf1071d8>] (PMGR_PROC_write+0x0/0xb4 [dsplinkk]) from [<bf109670>] (DRV_Ioctl+0x4bc/0x850 [dsplinkk])
r7:be9d5b9c r6:00008000 r5:c3161eb4 r4:00006c0c
[<bf1091b4>] (DRV_Ioctl+0x0/0x850 [dsplinkk]) from [<c00aafa4>] (vfs_ioctl+0x78/0x94)
r7:c2f4fa00 r6:00006c0c r5:be9d5b9c r4:c2f4fa00
[<c00aaf2c>] (vfs_ioctl+0x0/0x94) from [<c00ab630>] (do_vfs_ioctl+0x578/0x5d4)
r7:c2f4fa00 r6:00000003 r5:c2f4fa00 r4:c310e8a8
[<c00ab0b8>] (do_vfs_ioctl+0x0/0x5d4) from [<c00ab6cc>] (sys_ioctl+0x40/0x64)
[<c00ab68c>] (sys_ioctl+0x0/0x64) from [<c002cec0>] (ret_fast_syscall+0x0/0x28)
r7:00000036 r6:00008e00 r5:00000000 r4:00008eac
Code: f5d1f05c f5d1f07c e8b151f8 e2522020 (e8a051f8)
---[ end trace 054a240dbad44e88 ]---
I'm using Ubuntu 10.4 and TI MAKE system to build sources using DSPLink, both for GPP and DSP
EVM : DM6467T
CCSv 4.1
DSPLink 1.64
DVSDK 3.1
Windows 7 pro 64 bits
Does anybody have any suggestion ?
Thanks
CC