This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can L138 McBSP support AC97 AC-link interface/timing?

Other Parts Discussed in Thread: OMAPL138

From L138 TRM McBSP feature list, it supports:

AC97 compliant devices (the necessary multiphase frame synchronization capability is provided), 

Now customer want to connect with Cirrus Logic CS4299, the timing is as below:

It doesn't look like TDM mode also, and the AC-link has only 5 signal, FSR and FSX share same one, and is input to AC-97 codec, so I think below connect should not work with FSX and FSR connected together.

Question: How can McBSP work with AC-97 compliant devices like CS4299 .