This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to boot Vision SDK 2.10



We are unable to boot Vision SDK 2.10 on TDA2x with pre-built MLO as well as MLO generated by us.

Please find attached boot logs.

 TDA2xx SBL Boot

 DPLL Configuration Completed

 Clock Domain Configuration Completed

 Module Enable Configuration Completed

 TI EVM PAD Config Completed

 DDR Config Completed

 App Image Download Begins

 SD Boot - file open completed successfully

 MPU CPU0 Image Load Completed

 IPU1 CPU0 Image Load Completed

 IPU1 CPU1 Image Load Completed

 DSP1 Image Load Completed

 DSP2 Image Load Completed

 EVE1 Image Load Completed

 EVE2 Image Load Completed

 App Image Download Completed

 Putting MPU CPU1 in Off mode

 EVE MMU configuration completed

 EVE MMU configuration completed

 EVE MMU configuration completed

 EVE MMU configuration completed

*****************************************************************

 PMCCNTR counts once every 64 clock cycles, multiple by 64 to get actual CPU cyc                                                                                        les

 SBL Initial Config Cycles - 133859  (11.42 ms)
 SOC Init Cycles - 169431  (14.45 ms)
 DDR Config Clock Cycles - 43362  (3.70 ms)
 App Image Load Cycles - 48937008  (4175.95 ms)
 Slave Core Bootup Cycles - 207039  (17.66 ms)
 SBL Boot-up Cycles - 49491038  (4223.23 ms)
*****************************************************************

 Putting MPU in Retention...