Other Parts Discussed in Thread: TMS320C6678
Hi,
I am a Code Composer and TI newbie trying to learn the different abilities of the TMS320C6678 Evaluation Board. I am trying to follow the first example in the BIOS MCSDK 2.0 User Guide, creating Blink LED lights. I have tried other projects but always seem to encounter the same error with the library missing some Macro defines. I have created a source file as specified in the guide shown below. I have Code Composer 6.2.0 installed and PDK 3.0.0.
led_play.c
#include <cerrno>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include "ti\platform\platform.h"
#include "ti\platform\resource_mgr.h"
/* OSAL functions for Platform Library */
uint8_t *Osal_platformMalloc (uint32_t num_bytes, uint32_t alignment) {
return malloc(num_bytes);
}
void Osal_platformFree (uint8_t *dataPtr, uint32_t num_bytes) {
/* Free up the memory */
if (dataPtr) {
free(dataPtr);
}
}
void Osal_platformSpiCsEnter(void) {
/* Get the hardware semaphore.
* Acquire Multi core CPPI synchronization lock
*/
while ((CSL_semAcquireDirect (PLATFORM_SPI_HW_SEM)) == 0);
return;
}
void Osal_platformSpiCsExit (void) {
/* Release the hardware semaphore
* Release multi-core lock.
*/
CSL_semReleaseSemaphore (PLATFORM_SPI_HW_SEM);
return;
}
void main(void) {
platform_init_flags init_flags;
platform_init_config init_config;
platform_info p_info;
uint32_t led_no = 0;
char message[] = "\r\nHello World.....\r\n";
uint32_t length = strlen((char *)message);
uint32_t i;
/* Initialize platform with default values */
memset(&init_flags, 0x01, sizeof(platform_init_flags));
memset(&init_config, 0, sizeof(platform_init_config));
if (platform_init(&init_flags, &init_config) != Platform_EOK) {
return;
}
platform_uart_init();
platform_uart_set_baudrate(115200);
platform_get_info(&p_info);
/* Write to the UART */
for (i = 0; i < length; i++) {
if (platform_uart_write(message[i]) != Platform_EOK) {
return;
}
}
/* Play forever */
while(1) {
platform_led(led_no, PLATFORM_LED_ON, PLATFORM_USER_LED_CLASS);
platform_delay(30000);
platform_led(led_no, PLATFORM_LED_OFF, PLATFORM_USER_LED_CLASS);
led_no = (++led_no) % p_info.led[PLATFORM_USER_LED_CLASS].count;
}
}
led_play.cmd
-c -heap 0x41000 -stack 0xa000
/* Memory Map */
MEMORY {
L1PSRAM (RWX) : org = 0x0E00000, len = 0x7FFF
L1DSRAM (RWX) : org = 0x0F00000, len = 0x7FFF
L2SRAM (RWX) : org = 0x0800000, len = 0x080000
MSMCSRAM (RWX) : org = 0xc000000, len = 0x200000
DDR3 (RWX) : org = 0x80000000,len = 0x10000000
}
SECTIONS {
.csl_vect > MSMCSRAM
.text > MSMCSRAM
GROUP (NEAR_DP) {
.neardata
.rodata
.bss
}
load > MSMCSRAM
.stack > MSMCSRAM
.cinit > MSMCSRAM
.cio > MSMCSRAM
.const > MSMCSRAM
.data > MSMCSRAM
.switch > MSMCSRAM
.sysmem > MSMCSRAM
.far > MSMCSRAM
.testMem > MSMCSRAM
.fardata > MSMCSRAM
platform_lib > MSMCSRAM
}
I have the following screen shots of my project properties
The console error I get seem to indicate it cannot find the macro header during building though it appears to be setup perfectly from the example document.
Console:
**** Clean-only build of configuration Debug for project led_play **** "C:\\ti\\ccsv6\\utils\\bin\\gmake" -k clean DEL /F "led_play.out" "led_play.hex" DEL /F "led_play.d" DEL /F "led_play.obj" Could Not Find D:\MarkRoberts\led_play\Debug\led_play.out Could Not Find D:\MarkRoberts\led_play\Debug\led_play.obj 'Finished clean' ' ' **** Build Finished **** **** Build of configuration Debug for project led_play **** "C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all 'Building file: ../led_play.c' 'Invoking: C6000 Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-c6000_8.1.1/bin/cl6x" -mv6600 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-c6000_8.1.1/include" --include_path="C:/ti/pdk_c667x_2_0_2/packages" -g --diag_wrap=off --diag_warning=225 --display_error_number --preproc_with_compile --preproc_dependency="led_play.d" "../led_play.c" >> Compilation failure subdir_rules.mk:7: recipe for target 'led_play.obj' failed "C:/ti/ccsv6/tools/compiler/ti-cgt-c6000_8.1.1/include/s_c_features.h", line 439: warning #48-D: incompatible redefinition of macro "_STLP_VENDOR_CSTD" (declared at line 112 of "C:/ti/ccsv6/tools/compiler/ti-cgt-c6000_8.1.1/include/s_c__ti.h") "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 89: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 130: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 168: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 209: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 252: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 293: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 335: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 384: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 425: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 469: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 517: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_semAux.h", line 568: error #20: identifier "CSL_SEMAPHORE_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 110: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 184: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 232: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 289: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 332: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 375: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 418: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 467: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 507: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 551: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 594: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 652: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 695: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 731: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 768: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 804: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 841: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 892: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 939: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_xmcAux.h", line 974: error #20: identifier "CSL_DSP_DSP_XMC_CTRL_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 92: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 130: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 168: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 203: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 245: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 292: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 329: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 364: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 399: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 434: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 469: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 508: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 560: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 612: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 663: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 715: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 768: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 820: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 886: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 943: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1008: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1066: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1133: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1187: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1222: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1257: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1292: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1327: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1366: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1415: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1461: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1498: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1539: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1574: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1607: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1640: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1679: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1743: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1800: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1865: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1922: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 1986: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 2045: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 2096: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 2150: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 2202: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 2256: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined "C:/ti/pdk_c667x_2_0_2/packages/ti/csl/csl_cacheAux.h", line 2308: error #20: identifier "CSL_C66X_COREPAC_REG_BASE_ADDRESS_REGS" is undefined 80 errors detected in the compilation of "../led_play.c". gmake: *** [led_play.obj] Error 1 gmake: Target 'all' not remade because of errors. **** Build Finished ****
At this point I'm lost as to what to do. I've looked over the examples I could find in this forum and haven't had much luck. Anyone have any insight on what I may be missing? Thanks in advance.