Hi Experts,
Customer is trying to connect a device through DM365 EMIF on DM365 EVM.
They have following questions.
1) I cannot see in the EVM litterature how we would "connect" the signals from J23 to the processor pins. For example pin 6 of J23 is CPLD.CONN_GI06 and I cannot find which CPLD registers we need to configure that pin. Could you please clarify?
2) On the EMIF interface, I think I understand how it works but I am not sure which address space is available on the external connector (J14) and whether further address decoding is required or not. EM_CE0 and EM_CE1 are available on the connector but EM_CE0 is assigned to the Flash and EM_CE1 is used for the CPLD... Can you suggest which address space we should be using on the EMIF bus and how to decode it?