Other Parts Discussed in Thread: TMS320C6748
On the TMS320C6748, is it possible to turn on the EMIF clock and keep it running no matter how we use the EMIT interface (sync vs async)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320C6748
On the TMS320C6748, is it possible to turn on the EMIF clock and keep it running no matter how we use the EMIT interface (sync vs async)?
Herb
Can you clarify your query further
1) Are you trying to use the EMIFA clock (EMA_CLK) as an independent clock source/free running clock (rather then using EMIFA for SDRAM or Async memories)?
2) "Keep it running" implies what? Do you want to prevent it being clock disabled?
Assuming #1 , yes the EMA_CLK can be used as a free running clock (should not exceed 100 MHz), additionally even if you are using the EMIFA in asynchronous mode, you can still use the EMA_CLK (which is not needed for Async mode) for "other" functions.
You might find this post helpful
http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/p/52237/185319.aspx#185319
Regards
Mukul