We are using V4L2 in LSP 2.0 on a DM6441. We have our capture processing open the VPFE capture device, Queue some buffers, then start streaming while the imager is held in reset. Then we take the imager out of reset and ask the driver to DQUE a buffer. We can see that 1 1/2 frames have come out of the imager before the DQUE call returns. Our frame times are long and we can't afford the time wasted waiting for the driver to give back the frame. How can we eliminate the delay that seems to be built into V4L2?