Hi,
I immigrated immigrated to our project which based on dvsdk_3_10_00_16 and kernel2.6.32.
It can run,but the cpu occupation is too high.When I run "top".
CPU: 23% usr 16% sys 0% nic 0% idle 0% io 57% irq 3% sirq
So, I run "cat /proc/interrupts" .
CPU0
3: 0 AINTC dm365_h3a_af
6: 0 AINTC dm365_h3a_aew
8: 16391 AINTC davinci_osd
16: 444 AINTC edma
17: 884630 AINTC edma_error
32: 13462 AINTC clockevent
33: 0 AINTC free-run counter
39: 1013 AINTC i2c_davinci
40: 642 AINTC serial
42: 0 AINTC spi_davinci.0
52: 0 AINTC eth0
53: 6269 AINTC eth0
54: 10038 AINTC eth0
55: 0 AINTC eth0
Err: 0
I found out the irq 17 is abnormal.It is very low run the former program.
Can you tell me the reason?
Your prompt reply will be greatly appreciated.
Regards!