This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VIP V4L2 Sub Device

Other Parts Discussed in Thread: TVP5158

we are using Jacinto 6, In out platform there are multiple sources of video input (HDMI, TV Tuner etc...)   however, the control path is not used ( we don't use i2C etcc.)  the input source is connected via LVDS. the control path is routed not routed to Jacinto. In that case can we directly use the VIP driver ? do we need to define V4L2 sub device? or is it directly possible to the VIP driver available. without any modifications from TI.