Other Parts Discussed in Thread: OMAP-L137, CCSTUDIO, TPS65023
As per the document provided in the release DaVinci-PSP-SDK-03.20.00.13 in 50 page
For OMAP-L137 (or DA830, AM17xx)
When using CCStudiov3.3:
1. Start CCStudio v3.3.
2. From the menus, choose Project->Open.
3. Browse to the extracted ARM UBL source and open the ubl-omapl1x7.pjt project.
• To build for SPI Flash, select the "Config" option as BOOT_SPI in CCStudio window.
• To build for NAND Flash, select the "Config" option as BOOT_NAND in CCStudio window.
4. From the menus, choose Project->Build. When the build is complete:
• The Intel hex format binary (ubl-xxx.bin) file is generated in the Project Root directory.
• The executable ELF binary (ubl-xxx.out) file is generated in the Project Root directory.
• The Project Root directory is <armubl-install-dir>\ccsv3.3\
5. The files generated by the build procedure, have to be flashed.
• In case of DSP BOOT devices like OMAP-L137 or DA830, the Intel hex format binary file is suitable for
flashing.
when I try building(Build) the project i get an error as attached in the image! But rebuilding (rebuild)the code compiles
I am trying to do this to Check weather the .bin files gets generated or not as specified in the document
HELP REQUIRED ON THIS!
Thank you
Deepak R