Hi everyone,
I am currently building a custom am335x board and I am using version 2.00 of the processor sdk. My new board initially will have the eeprom blank. What is the easiest way to bypass the board detect checks in this version of the sdk? My template boards is the beagle bone black rev c so all the default initializations with respect to the BBB should work. If I do have to modify the source, can some one list which files (full path) I need to modify?
I build the u-boot source with:
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabhif- distclean
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabhif- am335x_evm_config
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabhif- u-boot.bin
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabhif- spl/u-boot-spl.bin
Thank you,
Ryan.