Other Parts Discussed in Thread: AM4372, AM4376
Team,
I have a customer that needs to migrate from the AM4376 (1GHz) to AM4372 (800MHz). They want to use the same pin mux file, will be using the same package, and do not currently use the PRU in the 4376. Can they use the exact same build image in the AM4372 as is being used in the AM4376? (booting from NAND, running Linux)
There is not currently any application issue they are worried about, but want to avoid testing a second image in the migration from AM4372 to AM4376. They are migrating to this part for production.
Anything at all they should check and change?
Thank you!