This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

evmdm6437 6437 audio processing

Dear sir,

Am doing audio processing on DM6437 with CCSv6.2,but i cant able to set the sampling frequency ,EVMDM6437_AIC33_setFreq(hCodec, 1) as we did in DSK6713[DSK6713_AIC23_setFreq(hCodec, 1)]............Here is my code and project,please let me know is my project is right and if not,let me know the changes.

thank you.

#include "evmdm6437.h"
#include "evmdm6437_aic33.h"

float filter_Coeff[] ={0.000000,-0.013457,-0.023448,-0.025402,-0.017127,-0.000000,0.020933,0.038103,0.043547,0.031399,
0.000000,-0.047098,-0.101609,-0.152414,-0.188394,0.805541,-0.188394,-0.152414,-0.101609,-0.047098,
0.000000,0.031399,0.043547,0.038103,0.020933,-0.000000,-0.017127,-0.025402,-0.023448,-0.013457,
0.000000


};

static short in_buffer[100];


static AIC33_Config config = {
       0, // 0  Page Select                     <- [Page=0]
READONLY, // 1  Software Reset                  <- [ResetOnly]
       0, // 2  Codec Sample Rate Select        <- [ADC=FS][DAC=FS]

    // For: [FS=48 kHz][MCLK=22.5792 MHz]
    0x92, // 3  PLL A                           <- [PLL=ON][P=2][Q=2]
    0x20, // 4  PLL B                           <- [J=8]
    0x6E, // 5  PLL C                           <- [D=7075]
    0x23, // 6  PLL D                           <- [D=7075]
    0x0A, // 7  Codec Datapath Setup            <- [FS=48 kHz][LeftDACPlays=left][RightDACPlays=right]

    0xC0, // 8  Audio Serial Data A             <- [BCLK=Master][WCLK=Master][3DEffects=OFF][DigitalMIC=OFF]
       0, // 9  Audio Serial Data B             <- [Mode=I2S][Length=16-bit][TransferMode=Continous]
       0, // 10 Audio Serial Data C             <- [DataOffset=0]
READONLY, // 11 Audio Codec Overflow Flag       <- [ReadOnly]
       0, // 12 Audio Codec Digital Filter      <- [OFF]

       0, // 13 Headset Detection A             <- [OFF]
       0, // 14 Headset Detection B             <- []

       0, // 15  Left ADC PGA Gain              <- [Mute=OFF]
       0, // 16 Right ADC PGA Gain              <- [Mute=OFF]
    0xFF, // 17 MIC3L/R to  Left ADC            <- [OFF]
    0xFF, // 18 MIC3L/R to Right ADC            <- [OFF]
    0x04, // 19  LINE1L to  Left ADC            <- [SingleEnd][Gain=0dB][Power=ON][SoftStep=OncePerFS]
    0x78, // 20  LINE2L to  Left ADC            <- [OFF]
    0x78, // 21  LINE1R to  Left ADC            <- [OFF]
    0x04, // 22  LINE1R to Right ADC            <- [SingleEnd][Gain=0dB][Power=ON][SoftStep=OncePerFS]
    0x78, // 23  LINE2R to Right ADC            <- [OFF]
    0x78, // 24  LINE1L to Right ADC            <- [OFF]
       0, // 25 MICBIAS                         <- [Power=OFF]

       0, // 26  Left AGC A                     <- [LeftAGC=OFF]
       0, // 27  Left AGC B                     <- [OFF]
       0, // 28  Left AGC C                     <- [OFF]
       0, // 29 Right AGC A                     <- [RightAGC=OFF]
       0, // 30 Right AGC B                     <- [OFF]
       0, // 31 Right AGC C                     <- [OFF]
READONLY, // 32  Left AGC Gain                  <- [ReadOnly]
READONLY, // 33 Right AGC Gain                  <- [ReadOnly]
       0, // 34  Left AGC Noise Debounce        <- []
       0, // 35 Right AGC Noise Debounce        <- []
READONLY, // 36 ADC Flag                        <- [ReadOnly]

    0xE0, // 37 DAC Power & Output Dvr          <- [LeftDAC=ON][RightDAC=ON][HPLCOM=SingleEnd]
    0x10, // 38 High Power Output Dvr           <- [HPRCOM=SingleEnd][ShortCircuit=OFF]
RESERVED, // 39                                 <- [Reserved]
       0, // 40 High Power Output Stage         <- []
       0, // 41 DAC Output Switching            <- []
       0, // 42 Output Driver Pop Reduction     <- []

       0, // 43  Left DAC Digital Volume        <- [Mute=OFF][Gain=0dB]
       0, // 44 Right DAC Digital Volume        <- [Mute=OFF][Gain=0dB]

       0, // 45 Line2L to HPLOUT Volume         <- []
       0, // 46 PGA_L  to HPLOUT Volume         <- []
    0x80, // 47 DAC_L1 to HPLOUT Volume         <- [Routed]
       0, // 48 LINE2R to HPLOUT Volume         <- []
       0, // 49 PGA_R  to HPLOUT Volume         <- []
       0, // 50 DAC_R1 to HPLOUT Volume         <- []
    0x09, // 51           HPLOUT Output         <- [Mute=OFF][Power=ON]

       0, // 52 LINE2L to HPLCOM Volume         <- []
       0, // 53 PGA_L  to HPLCOM Volume         <- []
       0, // 54 DAC_L1 to HPLCOM Volume         <- []
       0, // 55 LINE2R to HPLCOM Volume         <- []
       0, // 56 PGA_R  to HPLCOM Volume         <- []
       0, // 57 DAC_R1 to HPLCOM Volume         <- []
       0, // 58           HPLCOM Output         <- []

       0, // 59 LINE2L to HPROUT Volume         <- []
       0, // 60 PGA_L  to HPROUT Volume         <- []
       0, // 61 DAC_L1 to HPROUT Volume         <- []
       0, // 62 LINE2R to HPROUT Volume         <- []
       0, // 63 PGA_R  to HPROUT Volume         <- []
    0x80, // 64 DAC_R1 to HPROUT Volume         <- [Routed]
    0x09, // 65           HPROUT Output         <- [Mute=OFF][Power=ON]

       0, // 66 LINE2L to HPRCOM Volume         <- []
       0, // 67 PGA_L  to HPRCOM Volume         <- []
       0, // 68 DAC_L1 to HPRCOM Volume         <- []
       0, // 69 LINE2R to HPRCOM Volume         <- []
       0, // 70 PGA_R  to HPRCOM Volume         <- []
       0, // 71 DAC_R1 to HPRCOM Volume         <- []
       0, // 72           HPRCOM Output         <- []

       0, // 73 LINE2L to MONO_LOP/M Volume     <- []
       0, // 74 PGA_L  to MONO_LOP/M Volume     <- []
       0, // 75 DAC_L1 to MONO_LOP/M Volume     <- []
       0, // 76 LINE2R to MONO_LOP/M Volume     <- []
       0, // 77 PGA_R  to MONO_LOP/M Volume     <- []
       0, // 78 DAC_R1 to MONO_LOP/M Volume     <- []
       0, // 79           MONO_LOP/M Output     <- []

       0, // 80 LINE2L to LEFT_LOP/M Volume     <- []
       0, // 81 PGA_L  to LEFT_LOP/M Volume     <- []
    0x80, // 82 DAC_L1 to LEFT_LOP/M Volume     <- [Routed]
       0, // 83 LINE2R to LEFT_LOP/M Volume     <- []
       0, // 84 PGA_R  to LEFT_LOP/M Volume     <- []
       0, // 85 DAC_R1 to LEFT_LOP/M Volume     <- []
    0x09, // 86           LEFT_LOP/M Output     <- [Mute=OFF][Power=ON]

       0, // 87 LINE2L to RIGHT_LOP/M Volume    <- []
       0, // 88 PGA_L  to RIGHT_LOP/M Volume    <- []
       0, // 89 DAC_L1 to RIGHT_LOP/M Volume    <- []
       0, // 90 LINE2R to RIGHT_LOP/M Volume    <- []
       0, // 91 PGA_R  to RIGHT_LOP/M Volume    <- []
    0x80, // 92 DAC_R1 to RIGHT_LOP/M Volume    <- [Routed]
    0x09, // 93           RIGHT_LOP/M Output    <- [Mute=OFF][Power=ON]

READONLY, // 94 Module Power Status             <- [ReadOnly]
READONLY, // 95 Short Circuit Detection         <- [ReadOnly]

RESERVED, // 96                                 <- [Reserved]
RESERVED, // 97                                 <- [Reserved]

       0, // 98 GPIO1                           <- []
       0, // 99 GPIO2                           <- []
       0, // 100 Additional GPIO Control A      <- []
       0  // 101 Additional GPIO Control B      <- []
};


/*
 *  main() - Main code routine, initializes BSL and generates tone
 */

void main()
{
	AIC33_CodecHandle hCodec;

	Int32 l_input, r_input,l_output, r_output;

    /* Initialize the board support library, must be called first */
    EVMDM6437_init( );

    /* Start the codec */
    hCodec = EVMDM6437_AIC33_openCodec (0, &config);

    EVMDM6437_AIC33_setFreq(hCodec, 1);

       while(1)
        {	/* Read a sample to the left channel */
			while (!EVMDM6437_AIC33_read32(hCodec, &l_input));

			/* Read a sample to the right channel */
			while (!EVMDM6437_AIC33_read32(hCodec, &r_input));

				l_output=(Int16)FIR_FILTER(&filter_Coeff ,l_input);
 		 	    r_output=l_output;

			/* Send a sample to the left channel */
            while (!EVMDM6437_AIC33_write32(hCodec, l_output));

            /* Send a sample to the right channel */
            while (!EVMDM6437_AIC33_write32(hCodec, r_output));
        }

    /* Close the codec */
       EVMDM6437_AIC33_closeCodec(hCodec);
}


signed int FIR_FILTER(float * h, signed int x)
{
int i=0;
signed long output=0;

in_buffer[0] = x;  /* new input at buffer[0]  */

for(i=30;i>0;i--)
in_buffer[i] = in_buffer[i-1]; /* shuffle the buffer   */

for(i=0;i<32;i++)
output = output + h[i] * in_buffer[i];

return(output);

}



4846.fir.rar