This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HPI Bootloader issue on DSPC54x

Hi,

I designed a board in which I have a DSP C5402 connected to MSP430 MCU. After start-up, the MSP430 load the DSP FW sections to DSP Memory through HPI.

The interface have been working well. however, in some boards I got the issue that DSP is not performing bootloader correctly.

some useful details:

 - Hardware: HINT is tied to INT2, MP/MC pin connected to VSS.

- I tested the HPI read/write transactions >> It works fine.

- I'm able to run code on DSP through JTAG Link XDS.

-  both FW sections and Entry point are written to DSP correctly, However The DSP is not running FW.

My questions.

Is there any other thing That I should verify?

I need your help so I can debug if there is  HW or SW issue on the boards showing the issue.

Thanks.