This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Syslink crash while m3 loading



I am seeing syslink module crashes some time, while loading the m3 firmware.

Please find my crash logs below.

 [   12.690000] Internal error: Oops: 8000000d [#1]
 [   12.690000] last sysfs file: /sys/devices/virtual/gpio/gpio58/value
 [   12.690000] Modules linked in: dhd cfg80211 lib80211 compat syslink
 [   12.690000] CPU: 0    Not tainted  (2.6.37_DM388_IPNC_3.80.00 #1)
 [   12.690000] PC is at 0xebffffd0
 [   12.690000] LR is at Memory_alloc+0x78/0xac [syslink]
 [   12.690000] pc : [<ebffffd0>]    lr : [<bf014fac>]    psr: 60000013
 [   12.690000] sp : d7933e38  ip : 00000000  fp : d7933e64
 [   12.690000] r10: 431ca440  r9 : d7932000  r8 : bf0a1d18
 [   12.690000] r7 : bf0718d4  r6 : 00000034  r5 : 00000000  r4 : c0203914
 [   12.690000] r3 : ebffffd0  r2 : 00000004  r1 : 00000034  r0 : c0203914
 [   12.690000] Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
 [   12.690000] Control: 10c5387d  Table: 97d08019  DAC: 00000015
 [   12.690000] Process cappcontroller (pid: 181, stack limit = 0xd79322e8)
 [   12.690000] Stack: (0xd7933e38 to 0xd7934000)
 [   12.690000] 3e20:                                                       00000034 00000000
 [   12.690000] 3e40: 00000000 d8733c01 d7933e64 c018f35a 00000034 00000000 d7933e94 d7933e68
 [   12.690000] 3e60: bf01f240 bf014f40 00000034 60000013 d871e780 c018f35a d79d3580 431ca440
 [   12.690000] 3e80: 00000074 00000000 d7933efc d7933e98 bf045b4c bf01f1fc c018f35a 431ca440
 [   12.690000] 3ea0: 00000000 00000034 00000000 00000034 402a6280 00000000 d8732000 d7933ef0
 [   12.690000] 3ec0: d7933edc d7933ed0 d7933f3c d7933ed8 c00f633c c008dbe8 d81d7d00 00000027
 [   12.690000] 3ee0: 431ca440 00000027 00000000 00000000 d7933f74 d7933f00 c00d897c bf0459f0
 [   12.690000] 3f00: d871bd80 00000000 00000000 00000000 d7932000 00000001 d871bd88 00000002
 [   12.690000] 3f20: d80c0260 00000000 d7932000 00000000 d7933f6c d7933f40 c00cb2d0 c00f6138
 [   12.690000] 3f40: 00000000 d871bd80 00000001 00000000 d79d3580 431ca440 c018f35a 00000027
 [   12.690000] 3f60: 00000000 d7932000 d7933fa4 d7933f78 c00d8a48 c00d84b8 00000008 00000001
 [   12.690000] 3f80: 00000000 431ca440 20000054 00009019 00000036 c0048568 00000000 d7933fa8
 [   12.690000] 3fa0: c00483c0 c00d89fc 431ca440 20000054 00000027 c018f35a 431ca440 c018f35a
 [   12.690000] 3fc0: 431ca440 20000054 00009019 00000036 00000000 431cad88 00009019 00000001
 [   12.690000] 3fe0: 00000002 431ca438 4014bb18 40e2c1cc 60000010 00000027 98bfe021 98bfe421
 [   12.690000] Backtrace:
 [   12.690000] [<bf014f34>] (Memory_alloc+0x0/0xac [syslink]) from [<bf01f240>] (MessageQ_alloc+0x50/0xfc [syslink])
 [   12.690000]  r6:00000000 r5:00000034 r4:c018f35a
 [   12.690000] [<bf01f1f0>] (MessageQ_alloc+0x0/0xfc [syslink]) from [<bf045b4c>] (MessageQDrv_ioctl+0x168/0x848 [syslink])
 [   12.690000]  r8:00000000 r7:00000074 r6:431ca440 r5:d79d3580 r4:c018f35a
 [   12.690000] [<bf0459e4>] (MessageQDrv_ioctl+0x0/0x848 [syslink]) from [<c00d897c>] (do_vfs_ioctl+0x4d0/0x544)
 [   12.690000] [<c00d84ac>] (do_vfs_ioctl+0x0/0x544) from [<c00d8a48>] (sys_ioctl+0x58/0x7c)
 [   12.690000]  r9:d7932000 r8:00000000 r7:00000027 r6:c018f35a r5:431ca440
 [   12.690000] r4:d79d3580
 [   12.690000] [<c00d89f0>] (sys_ioctl+0x0/0x7c) from [<c00483c0>] (ret_fast_syscall+0x0/0x30)
 [   12.690000]  r8:c0048568 r7:00000036 r6:00009019 r5:20000054 r4:431ca440
 [   12.690000] Code: bad PC value

Not getting any clue, Please help me to debug.