Can the MPU be used to protect addresses that aren't in table 7-50 from the C678 data sheet?
Specifically, can it be used to protect the low memory addresses below the start of local L2 SRAM (0x00000000 - 0x007FFFF)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the MPU be used to protect addresses that aren't in table 7-50 from the C678 data sheet?
Specifically, can it be used to protect the low memory addresses below the start of local L2 SRAM (0x00000000 - 0x007FFFF)?
TI Experts-
If not, is there another way to do it ? We've got a corruption problem that takes up to 20+ hrs to occur, it's in a customer deployed location that we can't reach, and we really need to catch this at the "moment of impact". Corrupted pointers tend to lose their upper 2 bytes (see this thread) and we end up writing to low memory.
Any way to trigger on this is appreciated, thanks.
-Jeff
Signalogic