Hello everyone:
Just a simple question in regards to a full speed, self-powered, c6747 base USB peripheral we're designing. After my device goes through it's enumeration, I need to remove the 1.5k pullup on D+ line when the USB cable is unplugged. I can't seem to find any way of doing it via the registers documented in the USB 2.0 controller users guide. Do I have to resest and reinitialize the USB device to achieve this?
Thanks in advance for any answers provided.