This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5535 - Migrating from TUSB3200A

Other Parts Discussed in Thread: TMS320C5535

Part Number: TMS320C5535

Application: USB Audio Bridge

Question type: Development and troubleshooting

Support topic: /Product/Development and troubleshooting/Find resources for processor design/

Description of the problem: Hello,
I'm looking at moving from the discontinued TUSB3200A to the recommended replacement C55xx dsp.

Is it possible to have 6 USB audio channels from the host computer to the device (C55xx) and 2 from the device (C55xx) to the Host computer?

I purchased a TMS320C5535 eZdsp USB kit and was looking through the wiki on the C5000 Connected Audio Framework and it stated only stereo connections were available for version 1.52.

But I see you are currently on v02.00.02.04 . (Which I am having trouble installing.)

But anyway is it possible for the C55xx dsp to handle multiple channel usb audio and if it is not do you have any chip/dsp recommendations that handle it.

Thanks,
Matt