This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 and DM6467T DVSDK and Speed Options

Other Parts Discussed in Thread: CDCE949

Hey guys:

I am using the DM6467 and DM6467T and need documentation that clearly spells out what to do for the following speeds of operation:

1.)  DM6467 @ 594 MHz
2.)  DM6467 @ 729 MHz - my understanding that there is a hardware change required to get the video port to work properly (generate the proper 74.25 MHz video clock) since the internal 27 MHz clock can't generate the right clock speed per this DSP clock.  Is this correct and if so, where is this documented if that is the case?
3.) DM6467T @ 1GHz

So can I use DVSDK3.10 for each of these devices and if so, what specifically do I have to change in order to build for each of these devices?   The documentation that I have avaialble is not clear on these issues - please provide additional details.   Changes required to rebuild UBL, u-boot, uImage and/or DVSDK?  Please advise.

Thanks,
Tim