Hi Support,
For OTG mode, do NOT connect the USB0_ID pin, that is, leave the pin floating. Is this correct?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ikon,
ikon said:For OTG mode, do NOT connect the USB0_ID pin, that is, leave the pin floating. Is this correct?
Yes. That is correct.
For more detailed information please visit the section " 35.2.7 USB Controller Host and Peripheral Modes Operation" in the OMAPL138 TRM
Hi ikon,
ikon said:Q1. The “USB0_ID” (on OMAPl138) must be connected to the USB_ID pin (on the USB socket) in order for OTG to work, Is it correct?
yes, correct.
ikon said:Q2. If “USB0_ID” (On OMAPL138) was left open (No connection), which USB function can we achieve?a) Pure Host
b) Pure Device
c) OTG
If the USB0_ID pin is left open, it is OTG or device mode. It means, if you connect a pen drive, OMAPL138 will act as a host. If you connect the OMAPL138 into any of the USB HOST machine, then OMAPL138 will act as a peripheral.
If it is USB0_ID pin state is driven low or is grounded, the USB2.0 controller would assume the role of a host. This is pure Host / Forced host mode.