Other Parts Discussed in Thread: AM3352
Hi All,
U-boot version : 2013.01.01
SOC: AM3352
- The application is LED blinking application every 1 second the LED is going to ON and OFF, It's working Perfectly.
Now,
- I need to Load this application after U-boot, after u-boot control goes to the kernel, In that Kernel place i need to Load my application.
- I loaded the MLO , uboot.img and App.bin(my LED blinking application) to NAND flash, restart the Board, it's Not loading my app.
- rest again, stopped that u-boot # prompt load the Application bootm command
it's Prints Wrong Image format for bootm command
ERROR : can't get the Kernel Image.
- After that i checked the do_bootm.c file boot_cmd () function, in this function contain above prints not there.
- How to run my application After U-boot.
- Please specify which files i want to change in the u-boot 2013.01.01 version, to load the Application.
DDR3: H5TQ2G63FFR - PBC ,
U-boot loading address: on DDR3 is 0x80000000
Kernel loading address : on DDR3 is 0x80008000 ( i give the this load address to My app)
Please Specify the steps to load my application, I am the New for Boot loader.
Thanks in Advance.
regards,
Vamsi.