I have a question about TMDXBDKFP5515.
I can not afford to buy the TMS320C5515 JTAG emulator which is very expensive to load the program to TMDXBDKFP5515 platform which costs around $80.
But as I saw
in the TMDXBDKFP5515 description there is a PC application program for
communication with this platform using serial port, through the DB9
connection located over the platform.
Can anybody help me to know please,
1- Is it possible to use this serial interface to download the programs into the platform?
2- Is there any other way to load the DSP program to this platform without using the JTAG pod.
tnx,
Reza