Hi,
I have a question about AM335x GP EVM.
We have two EVM and those each boards revision is as follow:
//////////////////////////////////////////////
#1
-Base Board HW Rev.1.5C
-Daughterboard HW Rev.1.2B(CPLD Rev.1.0G)
-LCD Board HW Rev.1.3A
#2
-Base Board HW Rev.1.6A
///////////////////////////////////////////////
There are "Pin Use Assignment" file which can be dowload from following TI wiki.
processors.wiki.ti.com/.../AM335x_General_Purpose_EVM_HW_User_Guide EVM CPLD&tisearch=Search-EN#Pin_Use_Description
In this "Pin Use Assignment" file, it seem that it is appropriate to the following revision EVM.
////////////////////////////////////////////////////////////////////////////////
-Base Board HW Rev.1.1A-1.5A
-Daughterboard HW Rev.1.1A-1.1B(CPLD Rev.1.0D-1.0F),and HW rev 1.2A-1.2B(CPLD Rev.1.0G)
-LCD Board HW Rev.1.1A-1.3A
////////////////////////////////////////////////////////////////////////////////
As I mention above, our EVM Base Board revision are Rev1.5C and Rev1.6A.
Is this "Pin Use Assignment" file also appropriate to Rev1.5C and Rev1.6A GP EVM?
best regards,
g.f.