Hi
For our manufacturer request.
Could you please provide ESD level of DRA74x in MM model?
Because of only HBM and CDM level on the datasheet.
Note: The complete P/N is "DRA746APGABCRQ1"
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
For our manufacturer request.
Could you please provide ESD level of DRA74x in MM model?
Because of only HBM and CDM level on the datasheet.
Note: The complete P/N is "DRA746APGABCRQ1"
Mickey,
Do any of the following docs answer your questions?
JESD47I.01: Stress-Test-Driven Qualification of Integrated Circuits; JEP172A: Discontinuing Use of the Machine Model for Device ESD Qualification; JEP155: HBM Target Levels; JEP157: CDM Target Levels; JEP161: System Level Part 1 Overview; and JEP162: System Level Part 2 Design Methods
Thanks,
Dian