Hi,
I have been using AIF2's control and management (C&M) channels to configure RRHs via ipv4(ethernet) packets (like DHCP, TCP packets, and etc ..). I can simultaneously comminucate with 4 RRHs with each of them on different CPRI links. Each link has been configured to use different C&M channels such as LINK0 - CM0 or LINK1 - CM2.
Now, I need to do this for 6 LINKS (6 RRHs). Is there way to use 4 C&M channels to receive C&M packets "simultaneously" from 6 LINKS (6 RRHs) or send?. How should I configure AIF2 to achieve this and what was the reason for putting 6 CPRI ports but just 4 C&Ms?
AIF2 Driver : 01.02.00.00.
SDK: pdk_keystone2_3_01_01_04
SoC: TCI6638K2K
Regards,
Melih Bayraker