This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is "Arago file system" needed and if so, is it available

Other Parts Discussed in Thread: OMAP-L138

Hi,

I am using http://processors.wiki.ti.com/index.php/GSG:_Setting_up_OMAP-L1_Target_File_System to assist in using the ARM on the L138.

Under "prerequisites" it has "The Arago file system that is available at Arago Repository".

This is a dead link, so which is true:

      *Arago file system is required and can it be found somewhere else
      *Arago file system is required but not available
      *It is not required

Thanks!

Harry Thompson

  • While I do not know why that link is broken, it does look like there is a demo file system based on Arago on the SDK download page, under the OMAP-L138 - Linux heading. You will need some form of file system to properly boot the board, so I would go with your first statement as being true.

  • HI Harry, Bernie,

    This page probably needs updating as well. Ignore the broken link from the beginning of the page (I'm not sure who put it there). You will need a file system in there. David made some updates that are in RED for how to get the filesystem.

    Please see notes on the page:

    For PSP versions earlier than 3.20.00.11, the file system is found in the images/fs directory.

                 For PSP versions 3.20.00.11 or later, the file system needs to be downloaded sepeartely from the product download page into a temporary directory, such as /tmp.